Password Protection
Valid for S300, S400, S600, S700
Three ASCII commands serve for the password protection. These parameters can be set in the terminal screen of the setup software.
| PASSCNFG | sets the type of password protection |
|
PASSCNFG = 0 : with activated protection all write accesses to parameter are locked
|
|
|
PASSCNFG = 1 : with activated protection the command SAVE is locked only
|
|
| PASSX | sets the password |
| PASSX = 0 : no password protection | |
|
PASSX = y : sets password. Only numbers are allowed for password "Y"
|
|
| PASS | activates or deactivates the password protection |
|
PASS y : deactivates the password protection (y means the password)
|
|
|
PASS 0 : activates the password protection |
Example
PASSCNFG 1 PASSX 815 // amplifier write protected, password = 815 PASS 815 // write protection disabled PASS 0 // write protection enable
Home >
Knowledge Base >
FAQs >
Downloads >