Skip to main content

Kollmorgen Support Network

Convert AKD-B Parameter File to AKD-P >

Instructions to convert a saved AKD-B parameter file into an AKD-P file to load into an AKD-P drive.

KAS v3.06 is now available!! >

New Features Kollmorgen E-Bus Stepper Integration: AKT2G-SM-L50-000 - Stepper motor terminal with incremental encoder, 50 V DC, 5 A (Imax), 2 phases AKT2G-SM-L15-000 - Stepper motor terminal with incremental encoder, 24 V DC, 1.5 A (Imax), 2…

Procedures For Uploading and Downloading Drive Parameters With The S300 Drive >

Often users need to upload the parameters out of a failed drive and recommission a spare drive with the archived parameters. The attached documents detail these procedures. Note the documents assume you have the same model, hardware and firmware…

Real-Time AKD Current Limits Change Using KAS >

In many cases the AKD default peak currents have to be changed. There are several ways to do this, but not all are executed quickly and real-time. If AKD is working in standalone mode the easiest way is to declare the function 21 - Current…

EOT (End of Travel) Software Position Limits in a KAS application >

In a KAS PxMM application program, to setup software End Of Travel (EOT) position limits:

F40 Series Pac-Sci Motors to AKD >

Document to connect and run a F40 series Pac-Sci servo motor on the AKD drive. Note PDF below for downloading. 1. Select Feedback type 40, resolver. a. Verify position feedback poles = 2 b. Verify transformation ratio is 0.50 2. Wire…

SafeMotion Functions for S700 >

This article provides an overview of SafeMotion functions for Kollmorgen S700 servo drives.

KVB - How to change a recipe layout (add/remove tags or change datatypes on tags) without losing data >

With KVB, recipe data will get lost when adding/removing tags or changing data types on tags (variables). The following procedure outlines how to save the data for use with the changed layout:

AKD DRV.MOTIONSTAT Bits 11 and 15 >

Bits 11 “Motion task target position reached” and Bit 15 “Drive actual position is within the motion task target position window MT.POSWND” in the DRV.MOTIONSTAT are very similar. To clarify behavior, the bits in DRV.MOTIONSTAT (links point to…
Subscribe to Parameters