Modbus TCP to AKD BASIC program variables Quick Start Part 1: Modbus PollThis application note serves as a quick start with simple example using a Modbus Master simulator software called Modbus Poll to read/write over Modbus TCP to/from the AKD BASIC program ( variables ). This is part 1 of a two part series.
Boot Time of AKD / AKD2GThe boot time was measured from the point of applying 24V control power to the drives. The time was measured to specific indicators and functions of the drives.
Note that AC power was already turned on prior to running these tests, so that the drives could automatically enable. …
inglês
KAS v3.02 is now available!!New features include:
Enhanced AKD2G Drive Integration
Map EtherCAT feedback to PLCopen Digitizing Axis
Multiple IDE Instances
IDE Ease-of-Use Enhancements:
Elastic Search capability in On-Line help
See the article for more information.
Implementing Extended Multiturn on KAS (Non-Binary Gear Box)This article presents a solution for position loss in non-binary geared systems after a power cycle, a problem caused when the KAS controller overlooks the 12 multiturn feedback bits from the drive. A specialized User-Defined Function Block (UDFB) bypasses this limitation by directly reading the…
inglês
Touch Probe with the AKD EtherCAT driveThe touch probe feature of EtherCAT is simply a position capture. In fact, it uses the position capture feature in the AKD. When touch probe is set up and enabled, it automatically configures and arms the AKD’s position capture. There are two touch…
inglês
Configurando a Entrada Analógica no Drive AKDA entrada analógica dos drives AKD pode ser usada em diversas aplicações: como comando de corrente (torque), comando de velocidade, comando de posição, velocidade alvo da tarefa de movimento e para monitoração de limites de tensão do usuário.