Pular para o conteúdo principal

Search Articles

Modbus TCP Overview as it relates to the AKD driveModbus TCP is a communication protocol that is available on all models of the AKD drive ( except the AKD-P-NAPN or AKD-P-NBPN ( Profinet ).  The communication is supported on Ethernet physical hardware, the X11 Ethernet port on the top of the drive. inglês
Controlling Two Motors with AKD Dual Feedback SupportUsing both AKD feedback ports to support separate motors (individually) on a single drive. inglês
6445-001-N-N Fan UsageThe fan on the 6445-001-N-N & 6445-0001-K-N is designed to run continuously.If the fan stops it needs to be returned for repair.  If unit is left energized, it will damage a capacitor on the reset line. inglês
AKD drive losing the software enableThe software enable will go low on an AKD EtherCAT/CANopen drive whenever the drive's hardware enable is turned off or a fault condition occurs.  This is because the software enable is handled by the state machine in EtherCAT/CANopen.  The master controller must bring the inglês
Frequency Response Tuning Methods inglês
n12 warning on S300, S600, and S700Servostar drive n12 warning. inglês
S300 internal current resolution to trigger digital output mode 8 or 9For the S300, what is the resolution of the trigger point to turn outputs on based on a < or > of actual current?  This would relate to I<actO1TRIG and I>actO1TRIG in O1MODE=8 or O1MODE=9. inglês
Communicating with the AKD over Telnet using HyperTerminal and PuTTYNormally, the Workbench software is used to connect to and configure the AKD drives.  However, there may be some instances where Workbench can't be used or where another communication method is preferred for troubleshooting purposes, etc.  Two terminal programs t inglês
AKD Controlled Stop and Holding Brake Timing Table of Contents Description Configuratio inglês