Search Articles
| Cam Profile Creation in PLC codeAttached is a demo program showing an example of how to use cam creation function blocks to build a completely new profile while a program is running. The main function required is MLProfileBuild located in the function block library under Motion/Common > Profiles. This will create | inglês | |
| AKD F131 Emulated Encoder Line BreakThe AKD will generate a F131 fault when it detects that a channel, and it's complement, have a difference in voltage absolute magnitude greater than 0.2V / 200mV. | inglês | |
| How to Configure an AKD Drive with a Single Ended Incremental Encoder as the Primary Feedback DeviceWiring a single ended encoder to the AKD drive. | inglês | |
| S200 GUI and Windows 8.1 ProAs of June 17th, 2014, the existing S200 GUI softwares will not be capable of running with Windows 8.1 PRO. Nothing has been tested nor verified since 2011 when new software was developed for use with Windows 7. | inglês | |
| S600 Series Drive Connections for the Goldline EB Series Motors S600 Power Connector X9 | inglês | |
| S300 Series Drive Connections for the Goldline EB Series Motors S300 Motor Power Connector X9 | inglês | |
| S700 Series Drive Connections for the Goldline EB Series Motors S700 Series Drive Connections for the Goldline EB Series Motors | inglês | |
| Motor Inductance Range for 6410 Stepper DriveEvery now and then the question comes up as the inductance range the 6410 requires for stepper motor operation. The answer is none. The 6410 is not limited to a range of inductances. | inglês | |
| Using Hint3.exe to Download Firmware into the S600 DriveUpdating the S600 bootloader using Bint3.exe. | inglês |
Página inicial >
Base de conhecimento >
FAQs >
Downloads >