Salta al contenuto principale

Kollmorgen Support Network

Search Articles

AKD Basic Console Connection IssueIf the Console in the Basic programming screen in Workbench will not connect, try rebooting the AKD drive and rebooting the PC.  Also reboot any router or other networking devices that are used between the PC and the drive.   Inglese
KAS Webserver - Demonstration VideoAttached is a video demonstrating features of the PxMM web server. It can be accessed inside the IDE or directly from a web browser. Capabilities include: Inglese
Automation of the AKD Drive with the programmable Multi-Axis Master PxMM and a Siemens S7-1200/1500 PLC with Profinet and TIA V13The system covered includes a PxMM controller with up to twelve additional AKD drives. All automation functions are handled in the PLC, the functionality covers the following: Inglese
G&L Software ArchiveThe PiCPro and MMC lines (G&L Motion Control products) are obsolete and not available for new applications. Inglese
AKD Control Loop Update Rates Digital current controller (670 ns) Digital speed controller  (62,5 µs) Digital position controller (250 µs) Inglese
AKD DC Bus LinkThe DC bus link, or connections, of the AKD drive can be used to connect the DC bus of one drive to the DC bus of another drive.  The connection is done in parallel between two or more drives, with the maximum number of drives being limited by the total sum of the current ratings, as specifi Inglese
KAS HMI, obsoleteThis article provides information on obsolete KAS HMI panels. Inglese
Characteristic Data Safe Feedback Device Safe Hiperface Encoder EN 13849-1 EN 62061 PFHD (1/h) TM (years) MTTFD (years) Safe HIPERFACE Encoder SKS36S/SKM36S PLd, Kat.3 SIL CL2 1.3E-08 20 847 Inglese
AKD Safety Characteristic Data Device EN 13849-1 EN 61800-5-2 PFHD (1/h) TM (Years) Inglese