Search Articles
| Linear Actuators | Inglese | |
| De-tuning using the Workbench Performance Servo TunerHow to use the Performance Servo Tuner to de-tune the AKD The Performance Servo Tuner (or Autotuner) can be used even when the best tuning is not desired. When tuning to a lower than optimal performance level, we call it "de-tuning". | Inglese | |
| Connecting Two Motors to One DriveTwo Motors Can Be Mechanically Connected to a single Drive In this example DDL motors are used. However, linear, rotary, and permanent magnet motors also apply. | Inglese | |
| Reference Table AKM Connectors-Feedback Connector code (PTC) | Inglese | |
| EAC MarkingEAC is the abbreviation for Eurasian Conformity. The mark is used in the states of the customs union (Russia, Belarus, Kazakhstan) similar to the European CE mark. A manufacturer or supplier, who adds this mark to his product, declares | Inglese | |
| Encoder connector AKD-N View Contact socket | Inglese | |
| The Short Circuit Current Rating (SCCR) of the AKD Series Servo DrivesThe Short Circuit Current Rating (SCCR) of the AKD series servo drives is 42 kA. | Inglese | |
| S700 EEO Index Pulse Alignment Based on Feedback DeviceS700 EEO Index Pulse Alignment Based on Feedback Device | Inglese | |
| Setup of HALL feedbacksValid for S300, S700 | Inglese |
Home >
Supporto Prodotto >
FAQ >
Download >