Today’s servo-controlled machines are faster, smaller, and smarter than ever. As a result, machine users demand more and more performance, and this forces designers to keep improving their machines. Improving the servo performance of a machine can be challenging because so many factors come into play including the servo motors, the feedback sensor, the servo drives, and the mechanical transmission. This white paper is for designers who want to improve servo performance. It will walk you through the decisions you’ll need to make, starting with understanding how the servos affects the machine, which components have the dominant effects, and what changes are likely to make substantial improvements.
Fill out this short form
to view this White Paper
-OR-
Login / Register
to gain access to Kollmorgen content
1G Motion System
AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments
The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor phase-sequencing issues.
Engineer the Exceptional
Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.
Related Resources
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >
Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments >
The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor…
Kollmorgen introduces new high-voltage IC Ironcore DDL direct drive linear motor >
Discover Kollmorgen’s new linear direct drive motor, engineered to move heavy loads with fast precision and to simplify machine design for the global marketplace.
How can redundant servo feedback ensure fail-safe positioning when encoder failure isn’t an option? >
In medical devices, defense systems and many industrial applications, failure of the motion system is not an option. Learn how servo motors with integrated, redundant feedback devices simplify the challenge of assuring total motion reliability. Learn…
Accelerating the Development of Next-Generation Prostheses and Exoskeletons >
Learn how Kollmorgen servo technology is helping OEMs accelerate the design of next-generation prostheses and exoskeletons.
Kollmorgen and Stereotaxis Advance the Precision and Safety of Surgical Robots >
Kollmorgen’s advanced motion products and expertise are helping save and improve lives. Learn how the new Genesis surgical robot incorporates torque-dense AKM servo motors with specialized, integrated encoders to revolutionize cardiac ablation…
Direct Drive Technology Increases the Speed and Quality of Electric Vehicle Lithium-Ion Battery Production >
One important stage in manufacturing lithium-ion batteries for electric vehicles is seal-welding the positive-terminal top cap to the battery shell. Laser welding is the ideal technology for this purpose, but it requires precise motion, speed and…
Kollmorgen’s low-temperature servo technology simplifies cleaning of solar energy heliostats >
The development of photovoltaic and thermal solar energy—along with China’s rapidly growing capacity to manufacture them—has opened many new opportunities for sustainable energy production in international markets. At the same time, the demand for…