Skip to main content

Smart Mobile Robots at Philips >

Asti has implemented an AGV system for Philips, that uses Kollmorgen’s next generation technology.

MEQuadrat - Rotary Indexing Table - Providing orientation for materials >

Success Story: Swiss company MEquadrat AG builds test systems with decentralized servo technology from KOLLMORGEN.

VH Vertical Packaging - New potential with a separate labeler >

Why VH Vertical Packaging is developing its own solutions and why servo drives with 48 volts from KOLLMORGEN are the perfect match

Buehler - Pre-Ferment Application - A perfect solution in Bakery Automation >

For the pre-ferment, Bühler has developed a solution - JetMix - Better hygiene thanks to KOLLMORGEN’s stainless steel servo motor

Swiss Can Machinery - Filling Application - Anything but trivial: filling milk powder into cans >

Scaled technology and functioning interfaces are essential for Swiss Can Machinery / Hygienic drives from KOLLMORGEN

Opteq - Mobile Robots - Self-driving systems for internal material flow >

No name would have been more desirable. With the Packman 200, Opteq Robotics has developed a self-driving solution for material flows which makes its way quickly and directly through the aisles to reach its destination, just like the popular arcade…

OMET - Flexographic Printing Machine - Flexibility and Innovation for Top Printing Quality >

AKD-N decentralized drives and CDDR motors by Kollmorgen are the core of the innovative OMET Xflex X5, a printing solution with the best returns on investment in terms of market result of narrow web printing of labels and flexible packaging.

Mobile Robots (AGVs) in Hospital >

The new navigation technology simplifies the expansion of systems since no changes are needed in the infrastructure.

C.M.C. srl - Printing and Packaging Machine - An Excellent Press Mailing System >

PACKAGING DECENTRALIZED SOLUTION AKD N DRIVES AND AKM MOTORS FOR DIRECT MAILING AN EXCELLENT PRESS MAILING SERVICE Decentralizing the system to reduce space and materials   Promotional postcards and flyers, membership cards, coupons

Servo-Driven Injection Molding Machine Reduces Energy Consumption and Cycle Time >

Traditional injections molding machines use fixed-speed, three-phase motors that run continuously to drive the hydraulic pumps that power the machine. Excess hydraulic oil, which is especially generated during the “clamp hold” and “cooling” portion…

Todema - Printing Machine - For Automated Decoration >

CDDR Direct Drive and AKD PDMM Motion Controllers for accurate lacquering of screw caps

Mezit Technology - Industrial Digital Printing Machine Manufactured For the First Time in Turkey >

Digital Printing Accelerated With Contributions From Kollmorgen