Skip to main content

Lafer - Complete Motion Solution For Packaging >

COMPLETE MOTION SOLUTION FOR PACKAGING Schleck enjoy the aromatic double

Schleuter - Labeling Machine - 360 degree labeling with direct drive >

Motion Control and Direct Drives for labeling - 360 degree labeling with direct drive - Joint development: Motion control solution with integrated labeling controller

Kollmorgen - All in one: One cable for all applications >

All-in-One: Servo drives in single-cable technology - All in one: One cable for all applications - Single-cable technology in servo drives: More than ten years of practical experience

Multivac Relies on Kollmorgen for Pneumatic to Electric Transition >

Challenge: Transition from pneumatics to electrics to help improve controllability and reduce noise emissions, while increasing productivitySolution: AKM® Washdown and Foodgrade options with single cable technology, along with AKD® Servo Drives…

Multivac - Packaging Machine - Electrically Deep Drawn Packages: Faster Sealing Without Pneumatic (Europe) >

Quieter, more efficient and improved controllability: MULTIVAC uses Kollmorgen’s servo competency

Flat Glass, Double Edger “TITAN” Model Uses Proven Cost-Effective Motion Control Solution >

Challenge: Simplify machine design and reduce cost without sacrificing performance.Solution: AKD® PDMM based control system consisting of permanent magnet servo motors as well as induction motors with both open and closed loop functionality.

Candy Production is Transformed with a Proven Cost-Effective Motion Control Solution >

Challenge: Simplify the candy machine without sacrificing performance.Solution: Couple the AKD® PDMM with the KBM™ series motor to reduce the bill of materials.

Prinovis - Rotogravure Printing Press - How Prinovis Reduced Scrap, Increased Throughp ut and Ensured Future Flexibility with Dynamic Motion Solution from Kollmorgen >

In search of new controllers for register control of a rotogravure printing press, Prinovis Itzehoe GmbH implemented a new motion control solution from Kollmorgen that produced important, measurable results.

KAS™ Maximizes Productivity of Fully Automated Modular Paper Processing Machine >

The RC-500J jumbo roll collator, manufactured by the German-based Jakob Graphic Services GmbH, is raising the bar when it comes to processing a wide variety of printed continuous paper products.

Robust Design, Excellent Value, Higher Sales >

Challenge: Improve sales with an affordable stepper solution. Solution: K Series motor and P7000 drive which work cohesively together ensure optimal performance at excellent value.

Washdown Motors: Increase Longevity >

Challenge: Increase longevity of motor under high pressure washdowns and maintain cleanliness. Solution: Engineered sealed stainless steel motor and gearbox featuring feedback and power cables.

Reduce Costs and Improve Industrial Utility Vehicle Steering Performance >

Hydraulic steering systems have long dominated the industrial utility vehicle market because of their familiarity both to vehicle designers and operators. More recently, there’s been a trending toward the use of electronic steer-by-wire systems that…