Skip to main content
Success Story | 2 minute read

SUCCESS IN SPEED AND PERFORMANCE IN INDUSTRIAL DIGITAL PRINTING MACHINE

Industrial Digital Printing Machine Manufactured For the First Time in Turkey

Digital Printing Accelerated With Contributions From Kollmorgen

Kollmorgen Mezit Digital Printing Machine

Mezit Technology, a Bursa-based company, has manufactured an industrial digital printing machine for the first time in Turkey, in collaboration with Kollmorgen products and engineering. Following successful trials, the machine has started production. Mezit Technology officials state that the machine is 20% faster than its counterparts. The machine was manufactured as a result of R&D efforts that lasted around 6 months, and has been intensely sought-after by textile manufacturers from Turkey and from several other countries.

Kollmorgen Mezit Ibrahim Demir As owner of Mezit Technology, with substantial industry-specific experience in digital printing, Mr Ibrahim tells their start up story: “I have significant experience in the digital printing industry, and many years of expertise. During this time, I worked with several companies and learnt almost all the intricacies of this field. As a result of our evaluations, we decided that digital printing technology must be used more intensively in an important textile production centre like Turkey and even these machines must be manufactured in Turkey. We have diligently selected and gathered a technical team who will design and manufacture this machine, thus forming a highly experienced team.

Kollmorgen Mezit Linear Motor TechnologyWe turned to TUBITAK to develop this project, and after establishing collaboration within our team, we met with various companies to assess the market and to source materials and services. We came to an agreement with Kollmorgen for the motion control systems, and they delivered 1 linear direct drive motor, 5 servo motors, drives, boards and other control systems. We worked with 2 international companies for the software. We wanted to produce a technology meeting or exceeding the European standards, bringing together the best in the world, and we succeeded in manufacturing an industrial digital printing machine for the first time in Turkey. Our machine started production following the test phases, and one of the first clients has expressed how pleased they are with the machine so far”.

Kollmorgen project manager Seref Karaoglan summarises the motive behind their preferences in the project, and says, “It wouldn’t be inaccurate to say that Kollmorgen is cut out for this project. We are one of the few companies that could possibly manufacture all of the products used in the machine. Furthermore, I can easily say that we are the only company that is capable of providing a linear motor, and all of these products, while optimally utilising its engineering in such an important R&D project”.

Kollmorgen Mezit AKD and AKD PDMM Servo Drives 6 Axis Synchronisation with a Single Controller
Kollmorgen project manager Seref Karaoglan shares their success story in synchronisation, and says, “Another important element that we provided in the machine’s success is our AKD PDMM controller with outstanding features. Our controller is embedded in the drives; it simultaneously controls 6 axes that are comprised of pulling, bonding, band, head Y axes (linear motor), head Z axes and wiping (cleaning). This way, we were able to successfully ensure synchronisation between axes”.

Kollmorgen Mezit AKD PDMM Servo Drive20% Faster Than Its Counterparts
Mr Ibrahim from the Mezit Technology Company points out that the machine has the production capacity of 220-230 linear metres per hour, meaning that it is 20% faster than its counterparts across the world, and says, “So we can produce 400 square metres with 600x600 dpi quality. The total cost of R&D has reached approximately £360,000 (TRY 1.5 million). For now, we have production plans for just 2 machines, but we aim to manufacture 20 machines in 2016. We will establish dealerships in Brazil and China, and we are looking to develop opportunities farther afield, in other countries where the industry is dense”.

An Enviable Linear Motor Technology
Seref Karaoglan remarks that the most striking feature of the machine is its high speed, and that, “it is very important that it is able to reach desired speeds, while being able to stop in a very short time for pulling, bonding, band, head Y axes (linear motor), head Z axes and wiping (cleaning). I would like to highlight the quality of Kollmorgen at this point. It is capable of gaining very high momentum, as in order for the machine to carry out a successful process, it needs to reach 1.8 m/s in 150 milliseconds. Our high performance linear motor and servo drive and motion control solutions are able to address these needs”.

Emphasising that one of the most critical aspects of such machines is ‘the motion control’, the owner of the Mezit Technology company, Mr Ibrahim, indicates his reliance on Kollmorgen controllers and says, “Because there are so many synchronised motions, such as the simultaneous movement of units, the bonding of fabric to blanket, as well as drying-swinging in high speeds, this is a very complicated piece of technology. In this regard, Kollmorgen has met all of our expectations. We used symmetric printing technology in this machine and this was another important factor that increased our speed”.

Kollmorgen Mezit Seref KaraoglanAuthor: Seref Karaoglan
System Engineer Kollmorgen Elsim

 

 

 

 

About Kollmorgen
Kollmorgen is a leading supplier of integrated automation and driver systems, as well as related components, aimed at machine manufacturers all over the world. With over 70 years of experience in Motion Control Design and application, as well as its extensive knowledge in the areas of production standards and bespoke solutions, Kollmorgen provides prominent solutions in terms of performance, quality, reliability and ease of use. As a result, our clients gain indisputable leverage in the market. www.kollmorgen.com/uk

Download as PDF

AKD PDMM®

The AKD PDMM® combines one AKD servo axis and the PCMM EtherCAT master controller that supports up to 31+ more additional AKD axes.

  • Full KAS automation capabilities using IEC61131-3 soft PLC industry standard programming language
  • Integrated control for multiple servo axes, complete I/O and HMI interface
Learn More

Reduce Development Costs, Simplify Integration and Improve Performance of Packaging Machinery with AKD® PDMM

Reduce Development Costs, Simplify Integration and Improve Performance of Packaging Machinery with AKD® PDMMTechnology Brief - Q & A - Learn how AKD PDMM technology reflects changes and trends in the packaging industry.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Kollmorgen Automation Suite injects some pace into metalworking

Pipes cut to order >

Cut to length in no time at all, with no shavings and hardly any burs: Kollmorgen Automation Suite injects some pace into metalworking
Kollmorgen Automation and Motion Control - Full line catalog

Kollmorgen Full-line Catalog >

At Kollmorgen, we know that OEM engineers can achieve a lot more when obstacles aren’t in the way. With direct sales, engineering support, manufacturing facilities, and distributors spanning the Americas, Europe, the Middle East, and Asia, we’re…

Reduce Development Costs, Simplify Integration and Improve Performance of Packaging Machinery with AKD® PDMM >

Reduce Development Costs, Simplify Integration and Improve Performance of Packaging Machinery with AKD® PDMMTechnology Brief - Q & A - Learn how AKD PDMM technology reflects changes and trends in the packaging industry.

Designing for Manufacturability >

Designing for ManufacturabilityTechnology Brief - Capabilities Overview - Discusses how machine control systems that feature servo drives with built-in controllers deliver capabilities that significantly enhance productivity in manufacturing…

450 Blisters per Minute... PLC, Motion Control, and Drive as One Unit: A Complete Solution for PG Express >

Unparalleled innovations and passion to shape up the future of India is what best describes Kollmorgen. Not resting on its laurels, Kollmorgen exhibits relentless performance, ensuring reliability and quality by way of products and solutions it…

Flat Glass, Double Edger “TITAN” Model Uses Proven Cost-Effective Motion Control Solution >

Challenge: Simplify machine design and reduce cost without sacrificing performance.Solution: AKD® PDMM based control system consisting of permanent magnet servo motors as well as induction motors with both open and closed loop functionality.

Candy Production is Transformed with a Proven Cost-Effective Motion Control Solution >

Challenge: Simplify the candy machine without sacrificing performance.Solution: Couple the AKD® PDMM with the KBM™ series motor to reduce the bill of materials.

Schleuter - Labeling Machine - 360 degree labeling with direct drive >

Motion Control and Direct Drives for labeling - 360 degree labeling with direct drive - Joint development: Motion control solution with integrated labeling controller