Skip to main content
Success Story | 2 minute read

FOOD PROCESSING – BETTER HYGIENE THANKS TO AKMH

A perfect solution in Bakery Automation

For the pre-ferment, Bühler has developed a solution - JetMix - Better hygiene thanks to KOLLMORGEN’s stainless steel servo motor

Kollmorgen Bühler AKMH Stainless Steel Servo Motor

No hearty rye bread without sourdough. The stollen becomes deliciously soft when some of the baking ingredients are first mixed together and left to rise (thanks to the properties of yeast) before all the other ingredients are blended into the main dough. The mixture made mainly from cereal flour and bulk liquids such as water and milk is known as pre-ferment among bakers. With the JetMix, Bühler has developed a solution for the fully automated production of pre ferment and sourdough. By using AKMH stainless steel servo motors from KOLLMORGEN, Bühler successfully combined high productivity with maximum hygiene.

Kollmorgen Bühler JetMix ENCombine water and flour into a smooth and lump-free pre-ferment using dough hooks – this view is shared in domestic kitchens and among the medium-sized bakery sector. If the focus is on larger bakeries, then the JetMix is the ideal solution. The compact machine from Bühler does not combine water and flour mechanically, but through effective hydration. During this continual process, each flour particle is evenly hydrated by the finely atomized water spray. The result of this process has impressed users, mainly thanks to its high productivity and the quality of the fine and smooth preferment.

The quicker way to the perfect pre-ferment

The technical aspect of the JetMix consists of four servo axes: Two of them form the pump drive for the water and ensure the pre-ferment is pushed along. Each of these axes drives the dosing screw as well as the centrifugal stirrer. “There, the flour is accelerated radially so that we can create a perfectly formed ring from flour”, describes Heinz Lauermann, team leader of Material Handling Powder & Liquids at Bühler. The ring of flour that arises from the centripetal force reacts with the water spray in the mixing tube, which is introduced from the outside through fine nozzles by the servomotor driven pumps. The pressure is accurately regulated by the precisely operated servo drive. This precision is therefore necessary, because when the flour and water come into contact, they coalesce into a lump free dough. “Mechanical kneading methods for dough production are always associated with a high energy input. With the JetMix, the production of pre-ferment is significantly faster and more energy efficient”, emphasizes Lauermann. The Swiss works at Bühler’s Headquarters is in Uzwil.

Kollmorgen Bühler Heinz Lauermann EN Always enthusiastic about special ideas and alternative solutions, for Heinz Lauermann, the advancement of the JetMix, fitted with a stainless steel servomotor from KOLLMORGEN, which was first presented at a specialist trade fair in the USA, illustrates a highlight in the industry from a hygiene perspective. The most powerful of the four AKMH stainless steel motors drives the centrifuge that produces the ring of flour – comparable to a hand blender. “The broad speed control range of the motor helped us a lot during development to identify the correct speed for different types of flour and pre-ferments”. The finely balanced interplay between the spinning speed and the water spray being introduced with a pressure of up to 16 bar ultimately guarantees the perfect mixture – and can therefore also be stored as a tried-and-tested reproducible pre-ferment recipe in the control system. “If we had small drops rather than a fine spray, we would get lumps. Drops create lumps”, says Lauermann, who explains that after being mix in the JetMix, the pre-ferment is pumped into a storage tank for further fermentation. According to Bühler, the JetMix’s performance stands at 3.0 tons per hour. “If we multiply this amount by four, then we get the quantity of finished dough”. This makes 12 tons – and they are needed. The capacity of the ovens is especially large in industrial bakeries associated with discount stores. 100 to 120 tons of flour are processed daily for bread, bread rolls, cakes, and baked goods.

A high speed control range for production and cleaning

Kollmorgen Bühler EN JetMix Considering these quantities in a price-sensitive market with low profit margins, there is the risk that little attention will be paid to cleaning the machines. “This task reduces productivity. The longer the cleaning takes, the less the companies earn”. During the development of the JetMix, Bühler was adamant that it would be equipped for CIP i.e. that it must be attached to a central cleaning system (Clean In Place). The AKMH stainless steel motors from KOLLMORGEN must, therefore, operate at a high rotational speed, as that is required during the production phase. “That was an important discussion in the design of the drive system, to obtain a water velocity of up to 3 m/s, so that during cleaning, leftover dough does not remain stuck on the sides”. Moreover, the drive systems must deliver such a performance that they can even push a so-called pig through the pipes. This is shaped in a figure-of-eight, nestles up to the sides and pushes the dough caught in the pipe in to the fermentation tank. Bread factories waste less food because of this and do not excessively burden the CIP system or the local sewage plant. Furthermore, bread dough does not pass well through the sewage system and quickly begins to rot.

A more hygienic stainless steel motor with a single cable

Kollmorgen Bühler Single Cable Connection Technology Heinz Lauermann even describes the exterior handle of the AKMH stainless steel motors from KOLLMORGEN as pioneering. The use of stainless steel 1.4404 makes the AKMH series corrosion-resistant against aggressive cleaning products. The design of all the edges to have a radius of at least 3 mm and the surface finishes with a roughness of <0.8 μm prevents the accumulation of dirt. The AKMH stainless steel motors are connected by just one cable, including recirculation to the AKD servo drives, so that the installation of Bühler’s JetMix also contributes to the hygienic aspect. On the one hand, halving the cables halves time and space during installation and, on the other hand, is also an advantage for hygiene and operational safety. Using just one cable means soling and leaks are less likely. Kollmorgen AKD Servo Drive_m.png “Integrating the recirculation system in the motor cable was worked out very well by KOLLMORGEN”, acknowledges Heinz Lauermann. He describes a hygienic motor including “very perfectly rounded motor mountings”.

The compact units of sizes two to six are also used outside of the baking industry, especially in machine areas with direct product contact and aseptic processes. The AKMH stainless steel servo motor dissipates any lost heat effectively to the outside and therefore lowers derating. As a consequence, the FDA certified series, developed according to the EHEDG guidelines, supplies higher continuous torques at lower volumes.

The Bottom Line

Bühler’s JetMix clearly demonstrates how hygiene properties and cleaning capabilities of machines in the food industry can effectively be improved when stainless steel motors are used. It is not enough, however, to be satisfied with the material selection for the motor housings. Rather, the contour guide, connection technology and function must perfectly meet the requirements of Food Safety. “Our eyes have been opened from a hygienic perspective by AKMH”, summarized Lauermann.

 

Kollmorgen Martin Zimmermann Author: Martin Zimmermann, Key Account Manager Switzerland, KOLLMORGEN

 

ABOUT KOLLMORGEN
Since its founding in 1916, Kollmorgen’s innovative solutions have brought big ideas to life, kept the world safer, and improved peoples’ lives. Today, its world-class knowledge of motion systems and components, industry-leading quality, and deep expertise in linking and integrating standard and custom products continually delivers breakthrough solutions that are unmatched in performance, reliability, and ease-of-use. This gives machine builders around the world an irrefutable marketplace advantage and provides their customers with ultimate peace-of-mind. For further information please contact [email protected] or visit our website www.kollmorgen.com/uk

 

Download article as PDF

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments

The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor phase-sequencing issues.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

cost-optimized motion control

Reliable, Cost-Optimized Motion Control for Food Processing Washdown Applications >

Join this live webinar to discover how Kollmorgen Essentials™ Servo Drives (KED) paired with AKMA washdown motors and AKMH hygienic stainless‑steel motors deliver high‑performance, washdown‑ready motion across food contact, splash‑zone, and non‑food…
English, UK
Kollmorgen Essentials Servo Drives Bring Cost-Effective Servo Performance to Washdown and Hygienic Environments

Kollmorgen Essentials Servo Drives Bring Cost-Effective Servo Performance to Washdown and Hygienic Environments >

Kollmorgen Corporation, a global leader in motion control and automation solutions, has expanded the application range of its Kollmorgen Essentials™ Servo Drive (KED) to include hygienic and washdown environments.

Enhancing Washdown Motor Performance with a Unified, Cost-Optimized Motion Control System >

In this webinar, you’ll discover how the Kollmorgen Essentials™ Servo Drive (KED), combined with IP69K-rated AKMA anodized aluminum and AKMH stainless-steel servo motors, deliver reliable, high-performance motion at a value-driven price.
How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput

How Kollmorgen Motion System Powers a Cable Robot to Triple Throughput >

Learn why Rbot9 specified AKM2G servo motors and AKD servo drives to maximize the payload capacity, speed and vertical-load safety of its massive, suspended-cable robot.
AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments

AC PM Servo Drive Amplifiers: Different Servo Motor Phase and Commutation Alignments >

The issues with commutation alignment between servo motors and servo drives, especially when the motor and drive are from different manufactures can be quite challenging. Understanding typical design challenges can help you tackle motor…

Easy-to-Clean, Durable Motion Systems for Food Processing and Packaging >

The food processing and packaging industry plays a major role in ensuring that the final product is safe to consume. While food safety is a serious requirement, it also presents significant challenges for manufacturers. Frequent, high-pressure…

How can food packaging machine builders meet stricter food safety rules without sacrificing OEE? >

Clean and Productive — Improving Food Safety and Packaging Machine Reliability: Learn how food processing and packaging machines can endure direct washdown without the risk of damage to motion systems. Meet food safety requirements while maximizing…

Accelerating the Development of Next-Generation Prostheses and Exoskeletons >

Learn how Kollmorgen servo technology is helping OEMs accelerate the design of next-generation prostheses and exoskeletons.
Direct Drive Technology Increases the Speed and Quality of Electric Vehicle Lithium-Ion Battery Production

Direct Drive Technology Increases the Speed and Quality of Electric Vehicle Lithium-Ion Battery Production  >

One important stage in manufacturing lithium-ion batteries for electric vehicles is seal-welding the positive-terminal top cap to the battery shell. Laser welding is the ideal technology for this purpose, but it requires precise motion, speed and…