Skip to main content
Success Story | 2 minute read

PACKAGING: CDDR AND AKD PDMM FOR THE DECORATION OF BOTTLING CAPS AND CAGES

For Automated Decoration

CDDR Direct Drive and AKD PDMM Motion Controllers for accurate lacquering of screw caps

Kollmorgen Todema view of COLTAL

A fully servo-driven machine that can be used for various types of printing and lacquering. The machine has the capability to increase production whilst retaining high quality: today Todema meets the goal – Thanks to CDDR direct drive motors and to the KOLLMORGEN AKD PDMM motion controller.

Todeschini Mario Srl company, known by the brand name Todema (www.todema.it), was founded in 1960 in the province of Lecco and, since then, has acquired expertize in the manufacturing of industrial machinery and in the implementation of evolved automated systems. These automated systems include machines for the production of capsules,cages for bottling wine and other liquids, bending machines, lamination and printing systems, systems for the production of electro-welded chains, packaging systems and lines for the household appliances industry, as well as control systems that can be integrated in woodworking. The client portfolio ranges from a number of different industries, from the food sector to the metal and woodworking industry, and from different countries including Italy, Germany, Spain, USA, Argentina, Australia and New Zealand. During the past few years, the design and programming of automated and robotic lines has given a strong boost to the industrial processes covered by Todema.

“For this project, we contacted Kollmorgen because we needed to develop a system for colouring and printing screw caps for bottling wine and spirits. Our client required high-quality and production standards concerning rotogravure colouring, tampography, silk screen and hot foil printing. Our objective was to build a fully servo-driven machine, which was going to be a first of its kind in this sector,” Ing. Giovanni Todeschini, owner and Chief Technical Officer, explains.

“Following a technical and economic analysis, we decided to rely on Kollmorgen because they were able to offer torque motors system and the related controls that could be easily integrated with our technology. Quality, versatility and assistance have beaten the competition” (G. Todeschini).

The biggest challenge was to replace the traditional mechanical systems of our machine with mechatronic systems in order to obtain a new type of machine, which would be highly versatile and configurable by the client depending on their production needs. It was necessary to develop an integrated mechanical and electronic control system, achieving a seamless combination of the two engineering aspects. More specifically, the Todema design team, consisting of mechanical and electronic engineers, had to work quickly and systematically with KOLLMORGEN experts from the very first drafts of the project.

COLTAL MACHINE 
Kollmorgen Todema Coltal Machine Aluminium screw caps are largely used for bottling spirits, mineral waters, oil and most recently wines too. Todema provides COLTAL for the lacquering of cylindrical objects and capsules: lacquering and silk screen printing or embossing, from video, hot foil or tampographic with very high visual quality. COLTAL is effective on various materials, such as Tin, Aluminium, Plastic and Poly-laminated materials. An integrated servo-driven system fully controls the machine operation ensuring a check of the result even with variable or unforeseeable conditions, such as the different quality and level of deformation of the materials, the type of friction or the difference in dyeing.

Kollmorgen Todema Servo driven Coltal Machine

COLTAL machine technical specifications

SIZE  1250 X 980 X 2600 mm
PRODUCTION SPEED  3500-5500 pc/hour (depending on the type of printing)
SIZE OF CAPS  Diam. 28/32 mm; H 15/65 mm
DRYING  Hot air oven drying or UV LED system
PRINTING  Silk screen printing, painting, pad printing, hot foil printing on top, embossed printing on top
LOADING  Automatic, 3-way gravity force with linear conveyor belt
UNLOADING  Expulsion with pressure air directly in the box
INK RECYCLING  Integrated system to keep the ink level by means of 3+3 peristaltic pumps
MOTOR  CDDR motors
ACCESSORIES  Drying accessories
Video camera for checking the printing quality
Viscometer for ink density automatic control
Pallet machine for packaging the pieces.

 

Kollmorgen Todema Coltal Machine with CDDR Direct Drive

High performance in a small space: Direct Drive Cartridge DDR servomotors
In order to check the exact positioning of the two spindle-holding tables without further mechanical parts, two Direct Drive Cartridge DDR servomotors are used together with the related AKD drives. Such motors allow a direct control of the motion, thus eliminating all the mechanical transmissions that used to generate too much elasticity in the motion. In order to ensure the required precision, a direct-drive motor system was needed. Cartridge motors are the quickest and simplest solution to implement. The quality of printing and embossed lacquering depends on the precision and accuracy of the machine movements, which are provided by the torque motors and the related Kollmorgen control systems. The dis-posal of the mechanical transmission systems has considerably reduced the frequency of maintenance op-erations,need for spare parts and ease of maintaining the overall machine accuracy level over time.

Kollmorgen Todema CDDR Direct Drive

  • CDDR motor specifications:
  • 5-minute rapid mounting
  • 5 sizes ranging from 108 mm to 350 mm
  • The direct transmission of the forces without mechanical com-ponents greatly reduces operation and maintenance costs
  • 17 different lengths, 52 standard windings
  • Continuous torques ranging from 4.57 Nm to 510 Nm
  • Reduced cogging to enable a fluid rotation at low speed
  • Speed up to 2,500 rev/min
  • The play free set-up improves the system response
  • High-resolution integrated sinusoidal encoder (optional extra)
  • The rotor of the Cartridge DDR motor uses machine bearings and it transmits the torque by means of an innovative tightening system. Traditional components of mechanical transmission are no longer necessary

 

AKD PDMM: motion controller, PLC and servo-drive in a single device
Kollmorgen Todema AKD PDMM Servo DriveThe process is controlled by a smart AKD PDMM system with integrated PLC and motion control for the development of a virtual master for the generation of the main reference, and electronic cams for the positioning and motion sequential control. This key development, which has led to a great reduction of costs in terms of hardware and installation, as well as space needed in the electrical cabinet (up to 30%) and wiring reduction, was made possible due to the cooperation with KOLLMORGEN from the very first steps of this project.

The AKD servo amplifier combines innovative technology and outstanding performance within very small dimensions. These servo amplifiers with multiple features provide solutions for nearly any application, from basic torque and speed control, to register control, through to fully programmable multi-axis applications with embedded Kollmorgen Automation Suite™. Universal AKDs set the standards for efficiency and power density. The ADK series has been designed with the versatility, connectivity and power needed to increase the machine performance as well as the speed of integration. The motor setup mainly occurs through plug-and-play and offers a wide range of feedback. Among the various possibilities of Ethernet connection, options for both open and closed proto-cols are available. Online diagnostics and the data verification enable faster and error-free programming. A wider power range, enclosed in a compact design, allows you to use these robust drives with a single inter-face.

“Our client’s objective – Todeschini recalls – was a machine with a production of approximately 60/70 piec-es per minute. We largely exceeded that target”.  

Recap
“Our clients are highly satisfied with COLTAL – Todeschini points out –, the quality standards have been fully met and the production targets have exceeded our expectations by 15%. Kollmorgen staff worked with us painstakingly and quickly to ensure that the components that we used were highly reliable and high-performing. Our initial objective has been fully achieved and in fact we have highly exceeded our expectations particularly in terms of accuracy and quality”.

 

Kollmorgen Todema Ilario Manzi Author

 

Download article as PDF

 

 

Information about KOLLMORGEN
Kollmorgen is a leading provider of integrated automation and drive systems, as well as related components for machine manufacturers all over the world. With more than 70 years of experience in Motion Control design, application development and a strong knowledge in development of standard and special solutions, Kollmorgen had repeatedly provided top-of-the-range solutions in terms of performance, quality, reliability and ease-of-use, giving clients an actual marketplace advantage. For further information, contact [email protected] or visit our website www.kollmorgen.com/uk  

Download as PDF

Kollmorgen’s Direct Drive Technology Improves the Precision and Productivity of Lithium-Ion Battery Coaters

Direct drive technology improves the manufacturing quality and productivity of lithium-ion batteries used in battery-electric vehicles and other products that are changing the world.
Learn More

Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production

As electric vehicles promise cleaner, more sustainable transportation, the need for reliable lithium-ion batteries is skyrocketing. Battery manufacturers are looking for innovative ways to maximize production quality and speed.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

manufaturing facility with multi-axis motion control

Mastering Multi-Axis Motion Control in Modern Production Cells >

When motion systems scale, synchronization gets harder. Learn how modern production cells maintain precision, stability and throughput at speed.

How Cosmopack moved from specialized to flexible packaging solutions >

Learn how Cosmopack upgraded automated packaging line integration with decentralized motion architecture for more flexible packaging solutions.
Kollmorgen Automation Suite Brochure

Kollmorgen Automation Suite Brochure >

Premier machine automation programming package for high-performance motion and control in minutes

Kollmorgen’s Direct Drive Technology Improves the Precision and Productivity of Lithium-Ion Battery Coaters >

Direct drive technology improves the manufacturing quality and productivity of lithium-ion batteries used in battery-electric vehicles and other products that are changing the world.
Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production

Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production >

As electric vehicles promise cleaner, more sustainable transportation, the need for reliable lithium-ion batteries is skyrocketing. Battery manufacturers are looking for innovative ways to maximize production quality and speed.

Reducing Defects while Improving ROI in Metal Stamping with Direct-Drive Technology >

Compared to mechanical and hydraulic presses, mechanical servo metal stamping presses use high torque brushless motors to create more complicated stampings at faster speeds. But the type of motors used—a traditional geared or chain drive system or a…
Printing Machine

Direct Drive Motors Improve Flexographic Printing Performance >

Recent work done by Kollmorgen—a global leader in manufacturing motor and motion solutions—has shown that it is possible to synchronize components within the flexo printing process without mechanical transmission by using closed loop control…
Kollmorgen Automation Suite injects some pace into metalworking

Pipes cut to order >

Cut to length in no time at all, with no shavings and hardly any burs: Kollmorgen Automation Suite injects some pace into metalworking
KOLLMORGEN FREYMATIC LeanCut Machine Brick Industry

Bricks that can put in an appearance >

Motion Control by KOLLMORGEN makes fast and precise cuts from the column of clay