Skip to main content

Kollmorgen Support Network

Using KAS Project Starting Templates | 31 Jul 2020 | |

Using KAS Project Starting Templates

Starting with a project template saves the user development time. KAS Project Starter Templates contain:

  • code for programming motion and machine code
  • an internal control panel for developing and debugging programs
  • a HMI program to use with the Kollmorgen AKI HMI’s.

The user can then build on this foundation to complete their application. The following video reviews key features in the KAS project starting template.

Loading...

 

About this Article

C Wontrop