Skip to main content

Kollmorgen Support Network

AKD Basic using Single Precision Floating Point Decimal over Modbus >

Working with floating point decimal value conversions.

What is a Subnet Mask? >

A subnet mask is a bit mask used to define a subnet of an Ethernet network.  It acts like a filter to only allow devices with certain IP addresses to communicate. Subnets are used to specify which devices can communicate with which other…

KAS v3.06 is now available!! >

New Features Kollmorgen E-Bus Stepper Integration: AKT2G-SM-L50-000 - Stepper motor terminal with incremental encoder, 50 V DC, 5 A (Imax), 2 phases AKT2G-SM-L15-000 - Stepper motor terminal with incremental encoder, 24 V DC, 1.5 A (Imax), 2…

AKD and the Raspberry Pi >

Raspberry Pi Foundation and its background. The foundation's goal was to advance the Computer Science, Programming, and engineering education of children and adults with a low-cost and high-performance solution. From Raspberry Pi Foundation…

Reading of AKD axes position by Python and Raspberry Pi 3 Modell B >

This solution allows you to read the motor positions of three AKD axes using Raspberry Pi hardware and Modbus TCP/IP.

KVB Security Features Video >

The video embedded below goes through how to add security features with Kollmorgen Visualization Builder (KVB). Shows how to create accounts with different levels of security and how to make objects in HMI screens either hidden or disabled unless you…

Trio Motion Controller Modbus TCP Communications to AKD1G >

This application note demonstrates configuration and addressing for Modbus TCP communications using a Trio Motion Controller to AKD1G. The application notes is an example only and the implementation and verification of proper operation of the…

Automation Direct HMI Modbus TCP Communications to AKD1G >

This application note demonstrates configuration and addressing for Modbus TCP communications a Automation Drive HMI using their C-More Programming Software. The application notes is an example only and the implementation and verification…

Red Lion HMI to AKD1G using Modbus TCP >

This application note demonstrates configuration and addressing for Modbus TCP communications a Red Lion HMI using their Crimson 3.0 software. The application notes is an example only and the implementation and verification of proper operation of…
Subscribe to Modbus