Modbus TCP is a communication protocol that is available on all models of the AKD drive ( except the AKD-P-NAPN or AKD-P-NBPN ( Profinet ). The communication is supported on Ethernet physical hardware, the X11 Ethernet port on the top…
The Modbus protocol is a communications protocol that is based on a client-server architecture. It was created in 1979. In the industry, the Modbus has developed into a de facto standard since it is an open protocol.
Modbus allows connecting a…