Skip to main content

Kollmorgen Support Network

KAS - Mapping Hardware I/O | 28 Aug 2020 | |

KAS - Mapping Hardware I/O

The KAS IDE (Integrated Development Environment) has a straightforward way to connect I/O to variables in a kas project.  In a typical KAS system machine I/O can be connected to the PxMM controller via:

AKD Drive PxMM Controller AKT Remote I/O
image image image

The following video made a few years ago illustrates how I/O points from AKT remote I/O are connected to and utilized in a KAS application project. The process is similar for Kollmorgen drive and PCMM I/O.

Loading...

About this Article

C Wontrop