The AKT2G family is recommended for new applications requiring remote I/O in a PCMM or PDMM KAS application. This article and attachment compares the AKT2G Remote I/O family with the AKT Remote I/O family.
The KAS IDE (Integrated Development Environment) has a straightforward way to connect I/O to variables in a kas project. In a typical KAS system machine I/O can be connected to the PxMM controller via:
In a KAS project, the following outlines reading a thermocouple temperature in units of 0.1 Degrees C from a AKT-AN-200 or AKT-AN-400 slice I/O module. Note: Reading this note will help you get started working through other AKT thermocouple…