Skip to main content

Kollmorgen Support Network

G&L Software Service Packs | 28 May 2015 | |

G&L Software Service Packs

*IMPORTANT* - PiCPro V18.0 SP1 users

The automatic updating feature built into PiCPro will not work if run from PiCPro V18.0 SP1. Service pack 2 and greater will have to manually be downloaded from the appropriate section below. The automatic update function in PiCPro V18.0, with no service pack applied, will work correctly.

*IMPORTANT* - PiCPro V13, V14 and V14.1
PiCpro_auto_upgrade.pdf

Software Service Packs

Service Packs contain fixes for known bugs and contain no new features. In order for a Service Pack to install, the product's directory structure must be intact and the directories must contain the files originally installed by the product. If a Service Pack installation fails due to directory or file changes made by a user, the product will have to be uninstalled, re-installed and the Service Pack will have to be re-applied.

Click on a file to download. Save the file to a temporary location on your hard disk. After the download is complete, use Windows Explorer to find the file and double click on it to unzip. Choose a location to unzip to, then, when the file has unzipped, find the unzipped file, and double click the icon with the filename.exe to install (where filename is the name of the downloaded file).

Service packs are cumulative, meaning service pack 2 will contain service pack 2 changes plus all changes in service pack 1. Service pack 3 will contain service pack 3 changes plus all changes in service pack 2 and service pack 1.

Windows 7 and Windows Vista Note on Service Pack Installation:

After installing a service pack under Windows 7 or Windows Vista, a warning message may display from the Program compatibility Assistant: This program may not have installed correctly...

You will be given 2 choices: "Reinstall using recommended settings" and "This program installed correctly". Choose: "This program installed correctly".

PiCPro for Windows Professional Edition

Filename Description
PROV180S7.zip PiCPro for Windows V18.0 Professional Edition
Service Pack 7 - Released 02/18/2015, 7,732 KB
--- Service Pack 6 was an internal release only.
PROV180SP5.zip PiCPro for Windows V18.0 Professional Edition
Service Pack 5 - Released 02/28/2014, 6,973 KB
PRO180S4.zip PiCPro for Windows V18.0 Professional Edition
Service Pack 4 - Released 04/03/2013, 6,676 KB
PRO180S3.zip PiCPro for Windows V18.0 Professional Edition
Service Pack 3 - Released 08/21/2012, 6,530 KB
PRO180S2.zip PiCPro for Windows V18.0 Professional Edition
Service Pack 2 - Released 01/13/2012, 11,631 KB
PRO180S1.zip PiCPro for Windows V18.0 Professional Edition
Service Pack 1 - Released 03/22/2011, 4,216 KB
PRO170S1.zip PiCPro for Windows V17.0 Professional Edition
Service Pack 1 - Released 06/12/2009, 5,457 KB
PRO161S3.zip PiCPro for Windows V16.1 Professional Edition
Service Pack 3 - Released 06/17/2008, 15,922 KB
PRO161S2.zip PiCPro for Windows V16.1 Professional Edition
Service Pack 2 - Released 11/01/2007, 2,181 KB
PRO161S1.zip PiCPro for Windows V16.1 Professional Edition
Service Pack 1 - Released 06/29/2007, 541 KB
PRO160S2.zip PiCPro for Windows V16.0 Professional Edition
Service Pack 2 - Released 12/15/2006, 5,842 KB
PRO160S1.zip PiCPro for Windows V16.0 Professional Edition
Service Pack 1 - Released 11/06/2006, 4,342 KB
PRO151S3.zip PiCPro for Windows V15.1 Professional Edition
Service Pack 3 - Released 07/20/2006, 5,980 KB
PRO151S2.zip PiCPro for Windows V15.1 Professional Edition
Service Pack 2 - Released 07/12/2006, 5,979 KB
PRO151S1.zip PiCPro for Windows V15.1 Professional Edition
Service Pack 1 - Released 05/30/2006, 5,981 KB
PRO141S1.zip PiCPro for Windows V14.1 Professional Edition
Service Pack 1 - Released 11/19/2004, 3,904 KB
PRO140S2.zip PiCPro for Windows V14.0 Professional Edition
Service Pack 2 - Released 01/29/2004, 7,0247 KB
PRO140S1.zip PiCPro for Windows V14.0 Professional Edition
Service Pack 1 - Released 01/09/2004, 6,776 KB
PRO130S4.zip PiCPro for Windows V13.0 Professional Edition
Service Pack 4 - Released 03/28/2003, 6,874 KB
PRO130S3.zip PiCPro for Windows V13.0 Professional Edition
Service Pack 3 - Released 11/07/2002, 6,860 KB
PRO130S2.zip PiCPro for Windows V13.0 Professional Edition
Service Pack 2 - Released 09/10/2002, 4,184 KB
PRO130S1.zip PiCPro for Windows V13.0 Professional Edition
Service Pack 1 - Released 08/13/2002, 1,937 KB
PRO120S2.zip PiCPro for Windows V12.0 Professional Edition
Service Pack 2 - Released 10/30/2001, 3,926 KB
PRO120S1.zip PiCPro for Windows V12.0 Professional Edition
Service Pack 1 - Released 04/27/2001, 3,339 KB
pro110s1.zip PiCPro for Windows V11.0 Professional Edition
Service Pack 1 - Released 03/08/2000, 7,086 KB

PiCPro for Windows MMC Edition

Filename Description
MMCV180S7.zip PiCPro for Windows V18.0 MMC Edition
Service Pack 7 - Released 02/18/2015, 8,172 KB
--- Service Pack 6 was an internal release only.
MMCV180S5.zip PiCPro for Windows V18.0 MMC Edition
Service Pack 5 - Released 02/28/2014, 7,360 KB
MMC180S4.zip PiCPro for Windows V18.0 MMC Edition
Service Pack 4 - Released 04/03/2013, 6,676 KB
MMC180S3.zip PiCPro for Windows V18.0 MMC Edition
Service Pack 3 - Released 08/21/2012, 6,530 KB
MMC180S2.zip PiCPro for Windows V18.0 MMC Edition
Service Pack 2 - Released 01/13/2012, 12,071 KB
MMC180S1.zip PiCPro for Windows V18.0 MMC Edition
Service Pack 1 - Released 03/22/2011, 5,105 KB
MMC170S1.zip PiCPro for Windows V17.0 MMC Edition
Service Pack 1 - Released 06/22/2009, 5,623 KB
(This release addresses a fbinter.lib error that may have occurred with installation of previous V17.0 MMC SP1 release.)
MMC161S3.zip PiCPro for Windows V16.1 MMC Edition
Service Pack 3 - Released 06/17/2008, 15,613 KB
MMC161S2.zip PiCPro for Windows V16.1 MMC Edition
Service Pack 2 - Released 11/01/2007, 2,195 KB
MMC161S1.zip PiCPro for Windows V16.1 MMC Edition
Service Pack 1 - Released 06/29/2007, 540 KB
MMC160S2.zip PiCPro for Windows V16.0 MMC Edition
Service Pack 2 - Released 12/15/2006, 5,441 KB
MMC160S1.zip PiCPro for Windows V16.0 MMC Edition
Service Pack 1 - Released 11/06/2006, 3,904 KB
MMC151S3.zip PiCPro for Windows V15.1 MMC Edition
Service Pack 3 - Released 07/20/2006, 6,099 KB
MMC151S2.zip PiCPro for Windows V15.1 MMC Edition
Service Pack 2 - Released 07/12/2006, 6,098 KB
MMC151S1.zip PiCPro for Windows V15.1 MMC Edition
Service Pack 1 - Released 05/30/2006, 6,100 KB
MMC141S1.zip PiCPro for Windows V14.1 MMC Edition
Service Pack 1 - Released 11/19/2004, 3,776 KB
MMC140S2.zip PiCPro for Windows V14.0 MMC Edition
Service Pack 2 - Released 01/29/2004, 7,327 KB
MMC140S1.zip PiCPro for Windows V14.0 MMC Edition
Service Pack 1 - Released 01/09/2004, 7,073 KB
MMC130S4.zip PiCPro for Windows V13.0 MMC Edition
Service Pack 4 - Released 03/28/2003, 6,581 KB
MMC130S3.zip PiCPro for Windows V13.0 MMC Edition
Service Pack 3 - Released 11/07/2002, 6,534 KB
MMC130S2.zip PiCPro for Windows V13.0 MMC Edition
Service Pack 2 - Released 09/10/2002, 3,914 KB
MMC130S1.zip PiCPro for Windows V13.0 MMC Edition
Service Pack 1 - Released 08/13/2002, 1,694 KB
MMC120S2.zip PiCPro for Windows V12.0 MMC Edition
Service Pack 2 - Released 10/30/2001, 3,307 KB
MMC120S1.zip PiCPro for Windows V12.0 MMC Edition
Service Pack 1 - Released 04/27/2001, 2,836 KB
MMC110s1.zip PiCPro for Windows V11.0 MMC Edition
Service Pack 1 - Released 03/08/2000, 688 KB

PiCPro for Windows Monitor Edition

Filename Description
MONV180S7.zip PiCPro for Windows V18.0 Monitor Edition
Service Pack 7 - Released 02/18/2015, 8,589 KB
--- Service Pack 6 was an internal release only.
MONV180S5.zip PiCPro for Windows V18.0 Monitor Edition
Service Pack 5 - Released 02/28/2014, 7,772 KB
MON180S4.zip PiCPro for Windows V18.0 Monitor Edition
Service Pack 4 - Released 04/03/2013, 6,676 KB
MON180S3.zip PiCPro for Windows V18.0 Monitor Edition
Service Pack 3 - Released 08/21/2012, 6,530 KB
MON180S2.zip PiCPro for Windows V18.0 Monitor Edition
Service Pack 2 - Released 01/13/2012, 12,468 KB
MON180S1.zip PiCPro for Windows V18.0 Monitor Edition
Service Pack 1 - Released 03/22/2011, 5,094 KB
MON170S1.zip PiCPro for Windows V17.0 Monitor Edition
Service Pack 1 - Released 06/12/2009, 5,713 KB
MON161S3.zip PiCPro for Windows V16.1 Monitor Edition
Service Pack 3 - Released 06/17/2008, 15,919 KB
MON161S2.zip PiCPro for Windows V16.1 Monitor Edition
Service Pack 2 - Released 11/01/2007, 2,200 KB
MON161S1.zip PiCPro for Windows V16.1 Monitor Edition
Service Pack 1 - Released 06/29/2007, 541 KB
MON160S2.zip PiCPro for Windows V16.0 Monitor Edition
Service Pack 2 - Released 12/15/2006, 5,840 KB
MON160S1.zip PiCPro for Windows V16.0 Monitor Edition
Service Pack 1 - Released 11/06/2006, 4,314 KB
MON151S3.zip PiCPro for Windows V15.1 Monitor Edition
Service Pack 3 - Released 07/20/2006, 6,090 KB
MON151S2.zip PiCPro for Windows V15.1 Monitor Edition
Service Pack 2 - Released 07/12/2006, 6,089 KB
MON151S1.zip PiCPro for Windows V15.1 Monitor Edition
Service Pack 1 - Released 05/30/2006, 6,091 KB
MON141S1.zip PiCPro for Windows V14.1 Monitor Edition
Service Pack 1 - Released 11/19/2004, 3,877 KB
MON140S2.zip PiCPro for Windows V14.0 Monitor Edition
Service Pack 2 - Released 01/29/2004, 7,276 KB
MON140S1.zip PiCPro for Windows V14.0 Monitor Edition
Service Pack 1 - Released 01/09/2004, 7,031 KB
MON130S4.zip PiCPro for Windows V13.0 Monitor Edition
Service Pack 4 - Released 03/28/2003, 6,763 KB
MON130S3.zip PiCPro for Windows V13.0 Monitor Edition
Service Pack 3 - Released 11/07/2002, 6,705 KB
MON130S2.zip PiCPro for Windows V13.0 Monitor Edition
Service Pack 2 - Released 09/10/2002, 4,095 KB
MON130S1.zip PiCPro for Windows V13.0 Monitor Edition
Service Pack 1 - Released 08/13/2002, 1,871 KB
MON120S2.zip PiCPro for Windows V12.0 Monitor Edition
Service Pack 2 - Released 10/30/2001, 3,952 KB
MON120S1.zip PiCPro for Windows V12.0 Monitor Edition
Service Pack 1 - Released 04/27/2001, 3,351 KB
mon110s1.zip PiCPro for Windows V11.0 Monitor Edition
Service Pack 1 - Released 03/08/2000, 684 KB

Application Software

An application software upgrade to the PiCPro for Windows Applications package is a complete upgrade to the previous version. The 'readme' file associated with each upgrade describes what changes are included.

Filename Description
APP1802S1.zip Upgrade Release - PiCPro for Windows Applications V18.0.2
For PiCPro V18.0 SP1 (MMC/PRO)
Released 03/22/2011, 84,678 KB
APP1702S1.zip

Upgrade Release - PiCPro for Windows Applications V17.0.2 for PiCPro V17.0 SP1 (MMC/PRO)
Released 06/22/2009, 82,699 KB

This upgrade may not install correctly if a destination folder other than the default folder is selected.

APP1612S3.zip Upgrade Release - PiCPro for Windows Applications V16.1.2
For PiCPro V16.1 SP3 (MMC/PRO)
Released 06/23/2008, 67,425 KB
APP120S2.zip Upgrade Release - PiCPro for Windows Applications
Upgrade to V12.0-SP2.1 from V12.0.1-SP1.1
For PiCPro for Windows V12.0-SP1 (MMC/PRO)
Released 10/30/2001, 4,726 KB
APP120S1.zip Upgrade Release - PiCPro for Windows Applications
Upgrade to V12.0-SP1.1 from V12.0.1
For PiCPro for Windows V12.0 (MMC/PRO)
Released 04/27/2001, 4,723 KB
app1102.zip Upgrade Release - PiCPro for Windows Applications
Upgrade to V11.0.2 from V11.0
For PiCPro for Windows V11.0 (MMC/PRO)
Released 05/17/2000, 4,318 KB

OPC Server

Filename Description
OPC20S2.zip OPC Server V2.0
Service Pack 2 - Released 07/06/2000, 212 KB

MMC for PC Support Software

Filename Description
MMCS20S1.zip MMC for PC Support Software V2.0
Service Pack 1 - Released 08/13/2002, 189 KB

 

About this Article

dmcleod