MMC for PC Support Software V2.0-SP1 Windows 2000/XP

IMPORTANT

It is important to read this document. It provides late-breaking product information such as:

 

TABLE OF CONTENTS

 

TECHNICAL SUPPORT

For technical support call Giddings & Lewis at 1 800 558 4808, press 4 to speak to an engineer.
You can also send an e-mail to glmotion.info@danahermotion.com.

Support links are provided in the Add/Remove software listing for MMC for PC. This includes a support email address and website link that contains any service packs (if available).

 

NEW FEATURES/CHANGES

Service Pack 1

Ladder Scan Control

Windows XP

 

SOFTWARE NOTES

For an MMC for PC Controller minimum system requirements are:

 

KNOWN PROBLEMS AND WORK AROUNDS

 

INSTALLING THE SOFTWARE

This installation installs the software required to support the MMC for PC hardware on Windows 2000/XP. These programs include the driver, Socket Server, and a status program, which allow you to view the basic functions and settings of the hardware.

The following steps install the software.

  1. Make sure the MMC for PC board is installed in the PC.
  2. Power on the PC.
  3. Log in as a user with administrator privileges.
  4. A 'Found New Hardware Wizard' will appear. Click on the 'Cancel' button.
  5. Install the software by executing Setup.exe program on the installation media. (This may run automatically after inserting the CD.) Double click on 'Install MMC for PC Support Software' and follow the installer instructions.
  6. If successful, the PC must be rebooted to complete the installation.
  7. Click on the MMC for PC status icon in the status area of the taskbar (by the clock). The display will indicate whether the hardware is connected or not.

 

REMOVING THE SOFTWARE

The following steps remove the software:
  1. Go to Windows Control Panel and choose 'Add/Remove Programs'.
  2. Select 'MMC for PC Support Software', and click the Change/Remove button. Follow the uninstaller instructions.

 

TROUBLESHOOTING