This document covers the basic support for the G&L products. It includes information on the three different edition levels of PicPro. Information on the different G&L files types and how to determine what version of firmware being used in…
Dear Expert,
Currently we have lot of MMC -A4 Plus (standalone) connected to HMI (Schneider) using Ethernet. Somehow the MMC Ethernet module is fail (this is the 3rd times in last 4 month). Sadly we no Ethernet module left in the…
Good afeternoon
Tenho uma duvida, queria saber qual software para programar esse plc, meu windows é XP SP3 32bit, se alguem puder me ajudar eu agradeço.
The PiCPro and MMC lines (G&L Motion Control products) are obsolete and not available for new applications. As alternatives, we recommend the Kollmorgen Automation Suite and the AKD line of servo drives, respectively.
I got a PicPro program that I am trying to open. When I try to open the program I got the popup below that states
Version of PiCPro speicfied for this project is not the version running that currently running
Refer to the Motion Solutions V4 Readme.pdf for installation notes and instructions for converting existing project files for use with the new version of Motions Solutions.
Filename
Motion Solutions V4.0.1 (Minimal…
New MMC-SDN Drive Support for PiCPro V18
If you are using PiCPro V18.0 SP2, SP3, SP4, SP5 you must use the firmware provided below.
Filename
Description
MMC-SDN Drive Support
MMC-SDN R105.zip
Filename
Description
FIR180S7.zip
Firmware released with PiCPro for Windows V18.0 SP7
Includes: PiC, MMC, MMC Smart Drive, MMC Digital, S200, DL-DIU, MMC-SDN, and SliceIO firmware