Kollmorgen is committed to sourcing components and materials from companies that share our values regarding respect for human rights, integrity and environmental responsibility. Kollmorgen is also committed to complying with Section 1502, in…
This application note demonstrates specifically with Digital MMC Smartdrive with Drive Resident Control Card to Modbus Poll and to KVB/AKI configured as Modbus Serial masters.
This application note demonstrates specifically with Digital MMC Smartdrive with Drive Resident Control Card to Modbus Poll and to KVB/AKI configured as Modbus TCP masters.
The PiCPro and MMC lines (G&L Motion Control products) are obsolete and not available for new applications. As alternatives, we recommend the Kollmorgen Automation Suite and the AKD line of servo drives, respectively.
Refer to the Motion Solutions V4 Readme.pdf for installation notes and instructions for converting existing project files for use with the new version of Motions Solutions.
Filename
Motion Solutions V4.0.1 (Minimal…
New MMC-SDN Drive Support for PiCPro V18
If you are using PiCPro V18.0 SP2, SP3, SP4, SP5 you must use the firmware provided below.
Filename
Description
MMC-SDN Drive Support
MMC-SDN R105.zip
Filename
Description
FIR180S7.zip
Firmware released with PiCPro for Windows V18.0 SP7
Includes: PiC, MMC, MMC Smart Drive, MMC Digital, S200, DL-DIU, MMC-SDN, and SliceIO firmware