Search Articles
| EnDat Table of Contents Reference General | inglês | |
| Temperature RatingThe temperature rating of material is another item typically determined by the environment. Each material type has its own limitations for operating temperature range. The actual rating is defined as the allowable conductor temperature the insulation can safely withstand. | inglês | |
| Voltage RatingVoltage rating for cables varies between standards. Typical voltage ratings for cables are 300V and 600V. CE requires the equipment or other installations to have insulation rating equal to the maximum circuit voltage applied to any conductor within the cable or raceway. | inglês | |
| FlexingAutomation has placed additional requirements on cable design. These applications typically require motion. Stationary applications do not require the added stress of cable motion. When designing a cable for motion, you must consider: | inglês | |
| Four Quadrant OperationA servo system capable of controlling velocity and torque in both positive and negative directions is known as having "four-quadrant" operation (see diagram below). | inglês | |
| Synchronism Table of Contents Concentricity Cogging | inglês | |
| AKM Motors with Micron GearheadsAssignment of RediMount adapters to AKM motors RediMount Adapters that fit to AKM Motors: | inglês | |
| Residual Current Protective Device Table of Contents General Function | inglês | |
| DESINA Color CodeDESINA is an abbreviation for DistributEd and Standardised INstAllation technology for machine tools and manufacturing systems. | inglês |
Página inicial >
Base de conhecimento >
FAQs >
Downloads >