Skip to main content
 

Introducing TBM2G Frameless Motors from Kollmorgen. Delivering performance, scalability, and design flexibility, the TBM2G Series is ready to meet your demands.

Learn more

Incorporating Frameless Motors Into an Environmentally Resilient Design

Daily washdowns, deep-sea submersion, high radiation, high vacuum, hazardous atmospheres: When a housed servo motor can’t provide the protection you need in a compact form factor, consider embedding a frameless servo motor. Read this white paper to learn how.

Learn More

Achieving Ultimate Motion Precision Using Frameless Servo Motors

Frameless motors aren’t just for robotic joints. Compact actuators, sensor system gimbals, submersible propulsion systems and other applications benefit from direct drive precision and compact design. Learn how to directly embed a frameless motor in your mechanism.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Robotic arm application

Integrating Frameless BLDC Motors for Next-Generation Robotics Innovation >

RobCo scaled its modular robotics platform using TBM2G frameless torque motors for robot joints, delivering high torque and speed in a compact design.
Achieving Precision and Higher Payloads with Compact Robotic Actuators

Achieving Precision and Higher Payloads with Compact Robotic Actuators >

HEBI Robotics boosts compact actuator torque and accuracy for industrial inspection and maintenance applications with Kollmorgen TBM2G frameless servo motors.
Signs You Should Consider a Frameless Motor in Your Machine

Signs You Should Consider a Frameless Motor in Your Machine >

Big machines require big solutions. Right? But what if higher-performance machines could benefit from compact, space-saving, lightweight, more efficient embedded solutions?
English, IN
Incorporating Frameless Motors Into an Environmentally Resilient Design

Incorporating Frameless Motors Into an Environmentally Resilient Design >

Daily washdowns, deep-sea submersion, high radiation, high vacuum, hazardous atmospheres: When a housed servo motor can’t provide the protection you need in a compact form factor, consider embedding a frameless servo motor. Read this white paper to…
Achieving Ultimate Motion Precision Using Frameless Servo Motors

Achieving Ultimate Motion Precision Using Frameless Servo Motors >

Frameless motors aren’t just for robotic joints. Compact actuators, sensor system gimbals, submersible propulsion systems and other applications benefit from direct drive precision and compact design. Learn how to directly embed a frameless motor in…
TBM2G Frameless Motors for Propulsion Systems and Extreme Environments

Tech Sheet: TBM2G Frameless Motors for Propulsion Systems and Extreme Environments >

Servo motors are often used in extreme environments — for example, submersible vehicle propulsion systems, spacecraft, semiconductor manufacturing under high-vacuum conditions, hygienic equipment subject to high-pressure washdowns, and more.
Embedding TBM2G Frameless Motors into Gimbal and Precision Actuator Systems

Tech Sheet: Embedding TBM2G Frameless Motors into Gimbal and Precision Actuator Systems >

A gimbal is a pivoting support that permits rotation of an object around an axis. Additional degrees of freedom can be obtained by combining or nesting two or more gimbals, with their axes of rotation at 90° apart.
Embedding TBM2G Frameless Motors into Compact Rotary Actuators

Tech Sheet: Embedding TBM2G Frameless Motors into Compact Rotary Actuators >

An electric rotary actuator produces rotary motion to drive a load. In its simplest form, a direct drive motor is coupled directly to the load. Often, rotary actuators also incorporate a gearbox to increase torque while reducing speed. Appropriate…
Have You Considered a Frameless Motor?

Have You Considered a Frameless Motor?  >

When most engineers think of a brushless DC servo motor, they’re likely to visualize a housing with a flange to accept mounting bolts, connectors to accept power and data cables, and a rotor shaft that couples to the load. That’s the most common…