Skip to main content

* All webinars are presented in English, unless otherwise noted.

*Classroom courses are taught in English and in-person at our office in Radford, Virginia, USA, unless otherwise noted.

Tips for Sizing and Programming Motion Control for Gantry Applications >

Webinar

Organizing an application design from concept to construction can be a tremendous task. Applications such as a gantry—a multi-axis structure that shares a load—require special attention in selecting and implementing components. Since most gantry…

Increasing Performance with Modern Inertia Matching >

Webinar

Unexpected motion can ruin products and lead to dangerous situations. But what if you could remove unwanted motion while decreasing motor size and increasing performance? Impossible? Not when you understand the effects of inertia on system…

How Customizable Cobot Design Can Help You Build A Successful Surgical Robotics Company  >

Webinar

Collaborative robots and AI are becoming increasingly important for surgeons who must perform extremely precise, often highly repetitive tasks. But surgical applications have unique performance and certification requirements that are not widely…

Bringing Performance and Reliability to Harsh Environments with Lightweight AKMA Motors >

Webinar

How do you meet the demands of everyday washdowns in a non-stainless-steel motor? How do you combine performance and versatility with outstanding value in a lightweight motor design? How do you determine which motor to specify in demanding…

Differentiating Braking Techniques for Your Servo System >

Webinar

Stop! An important command in a motion system. Often brakes are used to mechanically slow the system, but brakes are also used to hold the load in place. Each brake type serves a purpose. When you order a brake with your motor, do you know what kind…

How to Use Grounding, Shielding and Bonding to Reduce Electromagnetic Interference (EMI)  >

Webinar

Electromagnetic Interference, or “noise,” poses a challenge to motion control engineers. Because EMI can cause unintended movement, mitigating the noise of unwanted electromagnetic signals is essential for sustaining precise motion. While there are…

Motioneering for Frameless Motor >

Webinar

Sizing a traditional servo or stepper motor is simple with the Motioneering sizing tool, but what about sizing a frameless motor? Are there any special considerations for these parts? Learn just how easy it is to size frameless motors using…

AKD2G Quick Setup with Safe Torque Off & Advanced Configuration with AKD2G Dual-Axis with Functional Safety >

Webinar

The Mentor Session Series for AKD2G servo drives provides an interactive learning experience with instructor demonstrations that allow you to observe programming techniques and strategies. We will begin with how to set up the drive, then lead you…

Motion Made Easy for Your Military Robotic Application >

Webinar

As technology changes the way humans and machines interact, opportunities to put new robotic driven capabilities into the hands of the warfighter continue to emerge. In addition to military drones and exoskeletons other types of defense and security…

How to Design Collaborative Robots to Improve Cycle Time >

Webinar

Is production demand pushing your cobot design to its performance limit? Do rigorous operation requirements cause overheating? Would you like to design a cobot with no compromises to performance or cycle time? Join us to learn what design…

Painless Frameless: Implementing and Installing Frameless Motors >

Webinar

Are traditional motors constraining your machine design? Motors don’t have to be bulky to create dynamic motion. Frameless motors allow you to keep your sleek machine design, and they are easy to implement. Join us for this highly popular event—now…

TBM2G: Next-Generation Motion Using Optimized, Compact Frameless Motors >

Webinar

How do you get maximum torque at full speed without specifying an oversized motor? How do you avoid excessive temperatures without derating? How do you get all the performance you need in a compact form factor that pairs with readily available…