Skip to main content

AKMH™ Durable and Hygienic Servo Motors

Purpose-Designed Servo Motors for the Wash-Down Environment

AKMH™ Durable and Hygienic Servo Motors

Producing wholesome quality food is challenging work. In addition to designing and manufacturing creative and tasty products, a laser focus on food safety is necessary for food processing companies to survive and thrive. Effective sanitation of machinery and facilities is critical in the production of safe food products.

Food safety is impacted by the ingredient supply chain, ingredient and finished product transportation, facility design, machinery design, sanitation procedures and overall process control. Machinery that stores and processes raw ingredients or the finished product has a significant effect on the food processor’s ability to produce products that are uncontaminated or spoiled. This paper reviews solutions for applying electric motors in wash-down areas. Test and survey data indicate a demand for motors that are purpose-engineered to withstand daily cleanings without sacrificing durability, production time or cost.

Sanitation in Food Production Facilities

Sanitation procedures are as varied as the food choices we have in our society. Each food production facility must evaluate the possible points where products may become spoiled or contaminated. Evaluation and procedures to guard against problems are included in a series of documents entitled Hazard Analysis and Critical Control Points (HACCP). Procedures for cleaning machinery and facilities are also included in the HACCP documents. Machinery must be sanitized so that it is not only visually clean, but also clean on a microbiological level on a daily basis.

In a typical “ready to eat” meat facility, food is produced for 16 hours and then a third eight-hour shift is devoted to cleaning the machinery. The cleaning procedure includes a number of steps, such as:

  1. Bulk food debris is removed manually with high-pressure air or water.
  2. Equipment is pre-rinsed with hot water.
  3. Caustic foam having either basic or acidic properties is applied to the entire machine and walls of the facility.
  4. Foamed surfaces are manually scrubbed as necessary to remove any observed product.
  5. Flood rinsing with warm water is used on the machinery to remove the foam and remaining product.
  6. Equipment surfaces are swabbed to test and confirm that the equipment is clean. If surfaces fail the test, all or a portion of the cleaning procedures will be repeated on that equipment.
  7. Chemically active sanitizing agents are applied to the machinery.
  8. Cool water is used to thoroughly rinse the equipment.
  9. Final tests to ensure the equipment is microbiologically clean are conducted.
  10. USDA inspectors verify procedures and cleanliness of equipment.

While procedures vary depending upon the type of food being produced, these procedures are repeated on a daily basis, and any equipment used in these manufacturing areas should be purpose-designed to withstand these cleaning procedures. Electrical equipment used in these wash-down areas present a problem because of the continual use of large amounts of water, harsh chemicals and the temperature cycles that occur for electrical equipment during alternating production and wash-down periods. Even more challenging than electrical products that can be fully sealed are electric motors that require an effective seal around a rotating shaft.

Component and Material Selection

Component attributes are important for the purpose-design of electric motors in wash-down areas. The seal, cable gland and connector components used for these areas need to be selected or designed carefully. The components must endure not only incidental contact with water, cleaning agents and sanitizer, but must also be able to endure direct high-pressure spray and daily contact with these items.

Materials used in the motor body and cable jacket are important as well. For the motor body and shaft, stainless steel alloys like 316L provide excellent corrosion resistance in this environment. Coated motors or other treatments tend to flake and even degrade and become porous after a few weeks. Lower grades of stainless steel corrode, as well, and issues arise after a slightly longer period of time. Cable jacket material must withstand the caustic chemicals, the mechanical manipulation due to direct spray with high-pressure water, and the constant contact with moisture and liquid without absorbing any water. Certain formulations of Thermoplastic Elastomer (TPE) work well for this purpose.

Ingress protection tests that produce IP ratings can be useful (Table 1), but do not simulate the actual wash-down environment. Equipment should be designed to endure daily wash-downs, not just a controlled test that only lasts a few minutes.

Thermal Cycles

Electrical equipment produces heat when operated. The space inside a servo motor can heat up to 140ºC (248ºF) during normal operation. When the production time is over and the machine is turned off the temperature inside the motor rapidly declines toward the ambient room temperature, which could be refrigerated and as low as 0ºC (32ºF). The temperature reduction in a sealed space creates negative pressure or a vacuum relative to conditions outside of the motor. Measurements of up to 5.5 PSI of vacuum have been documented during this cycle, which is revived slowly by air being pulled in through the seal or cable gland (Table 1). However, during that time the motor is being sprayed with water and cleaning chemicals that can be drawn into the motor along with the air. This vacuum needs to be released in another manner. The motor must be vented, which prevents this vacuum from developing. When a small tube is run through the motor cable to an area with clean dry air, like the control cabinet, the relative vacuum in the motor can be decreased to zero (Table 2).

Permanent or Temporary Covers

A typical method to deal with the durability problems discussed previously is to protect the motors with permanent or temporary covers during wash-down. This appears to be a very good answer to the problem. If the motors are not exposed to water, cleaning chemicals and chemical sanitizers, they will be more reliable. However, the hygienic demands combined with the chaos of food manufacturing and machine cleaning make these solutions unattractive.

Permanent Covers

Two issues may arise when creating steel covers around electric motors. First, guards over the motors create dead spots or growth niches that are not easy to inspect or clean. Product can enter the permanent covers and the warm moist environment inside the cover becomes an excellent place for pathogens to grow, multiply and then migrate to product surfaces. If the guards are removed and cleaned during the machine cleaning cycle the motors become vulnerable to the general cleaning environment, and even with clear procedures, motors often still get sprayed while uncovered. In addition, if the covers are removed and the motors are washed-down they are likely to fail. Also, adding stainless steel covers to the machine adds cost, size, and complexity to the machine without solving the underlying problem.

Temporary Covers or Bagging

Another method of protecting motors during wash-down is to put plastic bags over them and then remove the bags after the more stringent wash-down of the machine is done, and wipe down the motors manually. The question remains, however, are the motors clean if this method is used? During a meeting of the Kollmorgen Advisory Council we asked this question of twenty-three leading food safety professionals. Nineteen of them had significant doubt concerning the process and the other four indicated that it took much longer to complete the process. Also, despite detailed instructions, the bags are often not applied at all, leaving the motors vulnerable.

Covers Are Not The Answer

Ingress Protection Ratings vs. Purpose Engineering

The International Electrotechnical Commission has established a set of testing standards (IEC 60529) for equipment (Figure 5). The IP rating that most closely simulates the wash-down environment is IP69K. The IP69K test requires that the component to be tested be placed on a turntable. High-pressure, 1160 to 1450 PSI, hot water 80ºC (176ºF) is sprayed through (4) specified nozzles placed 10 to 15 cm from the component at 0º, 30º, 60º and 90º angles.

The nozzles spray a minimum flow rate of 14 liters per minute as the turntable rotates for 2 minutes. The component must operate normally after the test, and when disassembled there must be no ingress of water into the component. While this is a rigorous test, it falls short of simulating the wash-down environment. The standard does not test in any way for corrosion caused by chemical cleaning, thermal cycles of the component during production and cleaning cycles or the repeated daily mechanical damage that can occur during high-pressure wash. While IP ratings can be useful, selection of motors or other components that are purpose-designed to withstand the wash-down environment is a better choice for ensuring durability and continued effectiveness in wash-down production areas.

Conclusion

The best solution for applying electric motors in wash-down areas is to use motors that are purpose-engineered to withstand daily cleanings. The Kollmorgen AKMH Hygienic and Durable motor is purpose-designed for the wash-down environment. The motor body and all exposed metal surfaces are made of 316L stainless steel; the cable jacket is made of a thermoplastic elastomer that can withstand the mechanical wear of high pressure wash, daily exposure to chemical cleaning agents, without degrading or absorbing water. The shaft seal and cable glands have been selected to withstand daily wash-downs as well. The challenge of the thermal cycles that occur during production and cleaning cycles has been accounted for with a tube in the motor cable that allows for vacuum relief during the cool down cycle of the motor without inducing water or chemicals into the motor.

Selecting purpose-engineered product for wash-down areas is the right path to follow to ensure continued production and decreased maintenance costs in wash-down areas.

Contact Us About AKMH View AKMH

 

About Kollmorgen

Since its founding in 1916, Kollmorgen’s innovative solutions have brought big ideas to life, kept the world safer, and improved peoples’ lives. Today, its world-class knowledge of motion systems and components, industry-leading quality, and deep expertise in linking and integrating standard and custom products continually delivers breakthrough motion solutions that are unmatched in performance, reliability, and ease-of-use. This gives machine builders around the world an irrefutable marketplace advantage and provides their customers with ultimate peace-of-mind.

For more information contact us, email [email protected] or call 1-540-633-3545

Fill out this short form

to view this White Paper

-OR-

Login / Register

to gain access to Kollmorgen content

Privacy Statement - By sending us your contact details you agree that your personal data/user behavior can be electronically stored and processed. If you no longer wish to receive the enewsletter, you can unsubscribe at any time.

CAPTCHA

Easy-to-Clean, Durable Motion Systems for Food Processing and Packaging

The food processing and packaging industry plays a major role in ensuring that the final product is safe to consume. While food safety is a serious requirement, it also presents significant challenges for manufacturers. Frequent, high-pressure washdowns are essential to keep machines free from pathogens, yet these washdowns are often incomplete, ineffective and damaging to motors and other equipment. Common practices such as shielding or bagging motors to prevent damage are extremely time-consuming. Direct washdown of equipment that is not properly designed to prevent water ingress can lead to premature failure. Irregular and rough surfaces can harbor pathogens that are difficult to remove. Eliminate all these issues by employing these best practices for the design of a more hygienic and productive machine.
Learn More

Stainless Steel Food Grade AKMH Series

The AKMH Series is built to withstand the most rigorous of washdown regimens. The combination of the AKMH’s IP69K construction and corrosion resistant materials make for a servo motor that will last the life of your machine.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

cost-optimized motion control

Reliable, Cost-Optimized Motion Control for Food Processing Washdown Applications >

Join this live webinar to discover how Kollmorgen Essentials™ Servo Drives (KED) paired with AKMA washdown motors and AKMH hygienic stainless‑steel motors deliver high‑performance, washdown‑ready motion across food contact, splash‑zone, and non‑food…
English, UK
Kollmorgen Essentials Servo Drives Bring Cost-Effective Servo Performance to Washdown and Hygienic Environments

Kollmorgen Essentials Servo Drives Bring Cost-Effective Servo Performance to Washdown and Hygienic Environments >

Kollmorgen Corporation, a global leader in motion control and automation solutions, has expanded the application range of its Kollmorgen Essentials™ Servo Drive (KED) to include hygienic and washdown environments.

Enhancing Washdown Motor Performance with a Unified, Cost-Optimized Motion Control System >

In this webinar, you’ll discover how the Kollmorgen Essentials™ Servo Drive (KED), combined with IP69K-rated AKMA anodized aluminum and AKMH stainless-steel servo motors, deliver reliable, high-performance motion at a value-driven price.

Easy-to-Clean, Durable Motion Systems for Food Processing and Packaging >

The food processing and packaging industry plays a major role in ensuring that the final product is safe to consume. While food safety is a serious requirement, it also presents significant challenges for manufacturers. Frequent, high-pressure…

How can food packaging machine builders meet stricter food safety rules without sacrificing OEE? >

Clean and Productive — Improving Food Safety and Packaging Machine Reliability: Learn how food processing and packaging machines can endure direct washdown without the risk of damage to motion systems. Meet food safety requirements while maximizing…

From the Factory to the Farm: Unleashing the Power of Kollmorgen's Servo Motor Technology >

As smart automation increases farm productivity, there is a need for powerful, precise motors that can handle a wide range of heavy-duty tasks, day in and day out. But even the most advanced technology doesn’t change the basic nature of farming.

Can You Integrate a Superior Motor into Your Existing Food and Beverage Production Line? >

Every machine designer wants to deliver the best possible performance. Especially in today’s food and beverage industry, the pressure for optimum throughput and quality means that every OEM is striving to engineer new systems that are the best of the…
Sleeger Success Story

Food Processor Meets Hygienic Requirements >

A company that specializes in creating cutting, placing and packaging machines looked to Kollmorgen for an innovative motor design. See how the AKMH motor met the strictest hygienic requirements and integrated with a third-party drive.
Kollmorgen webinar, What is a Servo Motor?

What is a Servo Motor? >

When researching motor options for an application, one type that often comes up is “servo” motor. Many manufacturers expand and add descriptions like AC and brushless. What do these terms mean and what exactly is a servo motor?