Skip to main content
Success Story | 2 minute read

JBT Portioning System Benefits from Kollmorgen Hygienic Motor Design.

Hygienic machine components should be designed to work with existing cleaning regimens, not against them. The AKMH™ Servo Motor is built to withstand the most rigorous wash-down regimens.

Challenge

JBT Corporation has been producing food industry machinery since the 1880s. Expanding upon the success of their DSI™ portioning systems, they sought to develop a new blade portioner that would be easy-to-maintain, easy-to-clean and use less floor space while continuing to utilize both DSI Q-LINK™ Software and BladeSense™ Software technologies for yield optimization and blade condition monitoring.

Solution

AKMH Benefits

  • Motor covers are not required, reducing machine size, cleaning time and sanitation risk
  • Motor and cables can be exposed to 2 - 12 pH cleaning solutions and high-pressure spray up to 1450 PSI
  • Motor is designed to be easily cleaned and can be applied very close to the product production surface
  • Motor has a two-year warranty against water ingress

Have Similar Challenges and Want to See Real Results?

Contact:
Eddie Yang, Product Line Manager
540-731-5643
[email protected]  

The result was the DSI DB20 Portioning System - an accurate, hygienic, easy to operate system suitable for a wide range of linear portioning applications. Machine maintenance requirements are reduced significantly using self-aligning belts and software that suggests replacement blades at the optimal time. In addition to reducing maintenance frequency, the system is designed for routine maintenance to occur quickly with conveyor belts or belt sections and blades designed to be safely replaced in a matter of minutes increasing machine uptime.

JBT Kollmorgen AKMH SuccessThe DB20 System is designed for easy hygienic cleaning with the application of the Kollmorgen AKMH™ IP69K servo motors which are directly coupled to the blades to allow for a compact yet open design of the cutting compartment. The AKMH servo motors deliver the excellent servo performance and are durable enough to be applied without bulky motor covers that complicate cleaning and maintenance procedures and add to machine size.

AKMH Stainless Steel Servo Motors can be cleaned with solutions ranging from 2 to 12 pH and high pressure spray up to 1450 psi, allowing them to be cleaned just like the rest of the machine and hence save valuable time. Kollmorgen’s AKMH motors are designed per guidelines EHEDG, 3-A and NAMI standards and are designed with a smooth 32µ surface finish, laser annealed nameplate, no external fasteners, no metal to metal seams, no flat surfaces and no nooks and crannies leaving no place for pathogens or food to hide.

“These motors reliably survive direct spray from sanitation personnel, eliminating the troublesome housing and ventilation systems present on other blade portioners,” said Jon Hocker, Director of Technology and Product Line Management, JBT Corporation.

In addition to the motors, the machine is designed with ample lighting and open surfaces for inspection and cleaning and low profile removable trays for easy collection and clean-up of any minor cutting debris. The DB20 portioner can operate at belt speeds up to 100 feet per minute and perform up to 2200 cuts per minute, increasing production rates.

The Kollmorgen AKMH motor enabled the innovators at JBT to move their machine design forward and to deliver additional value to their customers.

 

 Download article as PDF

 

About Kollmorgen
Since its founding in 1916, Kollmorgen’s innovative solutions have brought big ideas to life, kept the world safer and improved lives. Today, its world-class knowledge of motion systems and components, industry-leading quality, and deep expertise in integrating standard and custom products delivers breakthrough motion solutions that are unmatched in performance, reliability, and ease-of-use. This gives machine builders around the world an irrefutable marketplace advantage and provides their customers with ultimate peace-of-mind.

For more information, visit kollmorgen.com, email [email protected], or call 540-633-3545.

Easy-to-Clean, Durable Motion Systems for Food Processing and Packaging

The food processing and packaging industry plays a major role in ensuring that the final product is safe to consume. While food safety is a serious requirement, it also presents significant challenges for manufacturers. Frequent, high-pressure washdowns are essential to keep machines free from pathogens, yet these washdowns are often incomplete, ineffective and damaging to motors and other equipment. Common practices such as shielding or bagging motors to prevent damage are extremely time-consuming. Direct washdown of equipment that is not properly designed to prevent water ingress can lead to premature failure. Irregular and rough surfaces can harbor pathogens that are difficult to remove. Eliminate all these issues by employing these best practices for the design of a more hygienic and productive machine.
Learn More

Stainless Steel Food Grade AKMH Series

The AKMH Series is built to withstand the most rigorous of washdown regimens. The combination of the AKMH’s IP69K construction and corrosion resistant materials make for a servo motor that will last the life of your machine.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

cost-optimized motion control

Reliable, Cost-Optimized Motion Control for Food Processing Washdown Applications >

Join this live webinar to discover how Kollmorgen Essentials™ Servo Drives (KED) paired with AKMA washdown motors and AKMH hygienic stainless‑steel motors deliver high‑performance, washdown‑ready motion across food contact, splash‑zone, and non‑food…
English, UK
Kollmorgen Essentials Servo Drives Bring Cost-Effective Servo Performance to Washdown and Hygienic Environments

Kollmorgen Essentials Servo Drives Bring Cost-Effective Servo Performance to Washdown and Hygienic Environments >

Kollmorgen Corporation, a global leader in motion control and automation solutions, has expanded the application range of its Kollmorgen Essentials™ Servo Drive (KED) to include hygienic and washdown environments.

Enhancing Washdown Motor Performance with a Unified, Cost-Optimized Motion Control System >

In this webinar, you’ll discover how the Kollmorgen Essentials™ Servo Drive (KED), combined with IP69K-rated AKMA anodized aluminum and AKMH stainless-steel servo motors, deliver reliable, high-performance motion at a value-driven price.

Easy-to-Clean, Durable Motion Systems for Food Processing and Packaging >

The food processing and packaging industry plays a major role in ensuring that the final product is safe to consume. While food safety is a serious requirement, it also presents significant challenges for manufacturers. Frequent, high-pressure…

How can food packaging machine builders meet stricter food safety rules without sacrificing OEE? >

Clean and Productive — Improving Food Safety and Packaging Machine Reliability: Learn how food processing and packaging machines can endure direct washdown without the risk of damage to motion systems. Meet food safety requirements while maximizing…

From the Factory to the Farm: Unleashing the Power of Kollmorgen's Servo Motor Technology >

As smart automation increases farm productivity, there is a need for powerful, precise motors that can handle a wide range of heavy-duty tasks, day in and day out. But even the most advanced technology doesn’t change the basic nature of farming.

Can You Integrate a Superior Motor into Your Existing Food and Beverage Production Line? >

Every machine designer wants to deliver the best possible performance. Especially in today’s food and beverage industry, the pressure for optimum throughput and quality means that every OEM is striving to engineer new systems that are the best of the…
Sleeger Success Story

Food Processor Meets Hygienic Requirements >

A company that specializes in creating cutting, placing and packaging machines looked to Kollmorgen for an innovative motor design. See how the AKMH motor met the strictest hygienic requirements and integrated with a third-party drive.
Kollmorgen webinar, What is a Servo Motor?

What is a Servo Motor? >

When researching motor options for an application, one type that often comes up is “servo” motor. Many manufacturers expand and add descriptions like AC and brushless. What do these terms mean and what exactly is a servo motor?