Setup Software
General
The servo amplifiers must be adapted to the requirements of your machine. Usually, you will not have to carry out this parameter setting yourself on the amplifier, but on a PC, with the assistance of the setup software. The PC is connected to the servo amplifier by a null-modem cable (serial). The setup software provides communication between the PC and the servo amplifier.
Workbench for AKD
![]() |
Workbench will run under WINDOWS 2000, XP (up to WB 1.15), Vista and WINDOWS 7 – 10. The functioning of the software has not been tested for WINDOWS running within Unix or Linux.
The latest version of the setup software can be downloaded from the Downloads page. |
DriveGUI for S300/S700
![]() |
DriveGUI.exe will run under WINDOWS 2000, XP, Vista and WINDOWS 7 – 10. The functioning of the software has not been tested for WINDOWS running within Unix or Linux.
The latest version of the setup software can be downloaded from the Downloads page.
The Online Help S300 S700 integrated in the software (incl. ASCII Object Reference) can be started independently. |
SafetyGUI for Safety cards S1-2/S2-2
![]() |
DriveGUI.exe will run under WINDOWS 2000, XP, Vista and WINDOWS 7 – 10.
The latest version of the setup software can be downloaded from the Downloads page.
The errors messages are described in file Error Codes. |
Drive for S400 / S600
![]() |
Drive.exe will run under WINDOWS 95c, 98, 2000, ME, XP, WINDOWS NT 4.0 and WINDOWS 7 – 10. The help system cannot be used with Windows 95a and 95b. Drive.exe will not work with WINDOWS 3.xx, DOS and OS2.
The latest version of the setup software can be downloaded from the Downloads page. The Online Help S400 S600 integrated in the software (incl. ASCII Object Reference) can be started independently. |
Home >
Knowledge Base >
FAQs >
Downloads >