Skip to main content

Kollmorgen Support Network

Reading a Drive Parameter with AKD EtherNet/IP | 25 Jan 2017 | |

Reading a Drive Parameter with AKD EtherNet/IP

This application note covers the different methods for reading a drive parameter over AKD EtherNet/IP.

Since it uses examples such as the MSG block for explicit messaging and AOIs ( add on instructions ) the article is specific to the AB Compactlogix and Contrologix PLCs ( Micrologix 1400 supports only Explicit Messaging ).

Dynamic Mapping and Explicit Messaging methods may also be valid for non-AB PLCs that support Ethernet IP but the user must confirm compatibility in this case. See the AKD EtherNet/IP Landing Page non-AB section for details if this applies to you.

 

About this Article

toddevans01