Cables



Part number scheme
Since 2012 the "talking" Part Number Schemes central / decentralized (AKD-C/N) helps with identifying the European cables.
Order codes for cables defined prior to 2012 and information for configuring cables can be found in the Accessories Manual.
Configured cables
We offer configured cables for the most important interfaces of our servo amplifiers, usually with DESINA Color Code.
![]() |
For Kollmorgen motors we deliver configured power cables with or without integrated brake wires. These cables are usable for trailing. |
![]() |
All Kollmorgen motors use feedback connectors. The both end configured feedback cables refer to the required pinout of servo amplifier and servo motor. These cables are usable for trailing. |
![]() |
For wiring AKM motors with SFD/DSL feedback, Kollmorgen offers Hybrid Cables. |
|
Different technologies for connecting the servo amplifiers to a PC or a network exist depending on the used servo amplifier model. In addition to the PC Connection Cables we offer adapters for multilink functionality (see page Multilink). |
![]() |
The cables are configured with high quality mating connectors. |
| Fieldbus Cables | For AKD servo amplifiers, Kollmorgen offers configured fieldbus cables for Ethernet and CAN connection. |
Home >
Knowledge Base >
FAQs >
Downloads >