Skip to main content

Kollmorgen Support Network

Setup of Unknown Motors >

Valid for S300, S700 (S400 & S600 minimal changes in display)

Cable Certification >

  Safety CCC CE UL UR cUL cUR EAC RoHS REACH SVHC Feedback Cable     EN / DE   yes   yes   EN & DE EN…

Debugging Intermittent EtherCAT Communication Issues >

The following fault, error, and alarm are each indicative of possible cable or connection problems. F125 on the AKD, "Fieldbus Sync frames lost." E30 in KAS, "EtherCAT communication failure during operational mode." A38 in KAS, "EtherCAT missed…

Bonding an AKMH Servo Motor Cable's Shield to the AKD's Ground (PE) Plate >

This article describes how to remove the outer cable jacket from the AKMH motor cable and solidly clamp it to the servo drive’s grounding bracket. For more information, see the application note: AKMH Cable Modification Application Note

EKM Motor Connectors and Corresponding Mating Connectors >

Kollmorgen does not offer power or feedback cables for the EKM series servomotors. Typically customer's will build their own cables for applications using the EKM motors. The EKM motor connector part numbers are shown in the EKM Catalog (attached to…

Cables >



Hybrid Cables >

Technical data of hybrid cables depends upon the cable material. US cables have different data from EU cables.

Accessories >

Industrial use of ever-faster and technically more complex servo drives in all areas of machinery, plant and equipment manufacture requires high-quality accessories. No EMC problems, safe drive operation, Plug-and-Play are guaranteed with the…
Subscribe to cable