Skip to main content

Kollmorgen Support Network

AKD Fault and Warning Messages | 07 Nov 2013 | |

AKD Fault and Warning Messages

Valid for AKD-B, AKD-P, AKD-T, AKD-M

The two digit LED display on the front panel of the drive shows the number of the fault or warning that occurred.

LED-akd.jpg

The left side of the LED displays "F" for a fault or "n" for warning.

The right side displays the fault or warning number as follows: 1-0-1-break. The highest priority fault is displayed on the LED. Multiple faults may be present when a fault condition is occurring. Check the AKD WorkBench Fault Screen for the entire list of active faults.

FaultMessage/WarningCauseRemedyDrive Response to Fault

..

 
  1. 24V Control Power input voltage dip.
  2. Auxillary encoder 5V (X9-9) shorted.
  1. Insure adequate 24V supply current capacity for the system.
  2. Check and fix X9 wiring.
  3. Check additional capacity for releasing the motor brake. An increased current consumption is expected which needs to be provided by the power supply.

N/A

F0

 

Reserved.

N/A

N/A

F101

 

Firmware incompatible.

Installed firmware is not compatible with the drive hardware.

Load compatible firmware into the drive.

Disable power stage

n101

The FPGA is a lab FPGA.The FPGA is a lab version FPGA.Load the released FPGA version that is compatible with the operational firmware.None

F102

Resident Firmware failed.

Software failure detected.

Restart drive. If issue persists, contact technical support.

Disable power stage

n102

Operational FPGA is not a default FPGA.The FPGA minor version is larger than the operational firmware default FPGA minor versionLoad the released FPGA version that is compatible with the operational firmware.None

F103

Resident FPGA failed.

Software failure detected. Load resident FPGA failure occurred (several cases according to flowchart, including incompatible image to FPGA type and fieldbus type).

Restart drive. If issue persists, contact technical support.

Disable power stage

F104

Operational FPGA failed.

Software failure detected. Load operational FPGA failure occurred (several cases according to flowchart).

Restart drive. If issue persists, contact technical support.

Disable power stage

F105

NV Memory Stamp.

Non-volatile memory stamp is corrupted or invalid.

Reset the drive to default memory values using Parameter Load in WorkBench.

Disable power stage

F106

NV Memory Data (might occur when downloading firmware).

Non-volatile memory data is corrupted or invalid. When this fault occurs after a firmware download, it is not an indication of a problem (clear the fault and perform a “save” to the drive).

Reset the drive to default memory values using Parameter Load in WorkBench.

Disable power stage

 

n107

Positive switch.

Positive position limit is exceeded.

Move the load away from the limits.

Controlled stop

 

n108

Negative switch.

Negative position limit is exceeded.

Move the load away from the limits.

Controlled stop

F121

Homing Error.

Drive did not finish homing sequence.

Check homing sensor, homing mode, and homing configuration.

Controlled stop

F123

n123

Invalid motion task.

Invalid motion task.

Check motion task settings and parameters to make sure that the values entered will produce a valid motion task.

Disable power stage

F125

n125

Fieldbus Sync frames lost.

The fieldbus lost synchronization.

Check fieldbus connection (X5 and X6 if you are using EtherCAT; X12 and X13 if you are using CANopen) or the settings of your EtherCAT or CANopen master.

Controlled stop

F126

n126

Bode plot too much movement.

Too much movement was created during a Bode plot. Motor is unstable and is not following drive instructions.

Check that the system is closed loop stable. Refer to the system tuning guide.

Dynamic braking

F127

Incomplete Emergency Procedure.

Incomplete emergency stop procedure (problem with the emergency stop motion task).

Disconnect power from drive and check emergency stop procedure.

Dynamic braking

F128

Mpoles / Fpoles not integer.

Ratio of motor poles to feedback poles must be a whole number.

Change to a compatible feedback device.

Disable power stage

F129

Fieldbus Heartbeat lost.

Heartbeat lost.

Check CANopen cabling. Reduce bus load or increase the heartbeat update time.

Controlled stop

F130

Secondary feedback supply over current.

5V power supply was shorted out on X9.

Check X9 connection.

Disable power stage

F131

Secondary feedback A/B line break.

Problem in secondary feedback detected.

Check secondary feedback (X9 connection).

Disable power stage

F132

Secondary feedback Z line break.

Problem in secondary feedback detected.

Check secondary feedback (X9 connection).

Disable power stage

F133

Fault number changed to to F138. See F138 for details.  Disable power stage

F134

Secondary feedback illegal state.

Feedback signals were detected in an illegal combination.

Check X9 connection.

Disable power stage

F135

n135

Fault on FB2 is preventing remote commutation for FB1.

Attempt to issue motion task before the axis is homed. Axis must be homed before motion task can start.

Change opmode or home axis.

Disable power stage

F136

Firmware and FPGA versions are not compatible.

The FPGA version does not match the firmware FPGA version constants.Load the FPGA version that is compatible with the firmware.Disable power stage

n137

Homing and feedback mismatchThe configured homing mode is not supported by the motor feedback type used.Change homing mode.None

F138

Instability during autotune.

Drive current (IL.CMD) or velocity feedback (VL.FB) exceeds allowable limit (BODE.IFLIMIT or BODE.VFLIMIT). This fault only occurs in BODE.MODE 5. This fault often occurs when complex mechanics, belts, and compliant loads are present.Change BODE.MODE if appropriate. If BODE.MODE 5 is appropriate and the fault occurs at the end of an Autotuning, then the motor is not robustly stable. You can manually adjust Autotuner settings. Manual tuning may be required to make the motor stable.Controlled stop
F139

Target position was overshot due to invalid motion task activation.

The drive cannot decelerate from its current speed to reach the end point of the second motion task without moving past it. Increase the deceleration rate in the move or trigger the move earlier.Change Motion task profile and clear fault with DRV.CLRFAULTS. Or change the value of FAULT139.ACTION = 1 to ignore this condition.Disable power stage
n140VBUS.HALFVOLT has changed. Save the parameters and reboot the drive.The user has changed the numerical value of VBUS.HALFVOLT. This change only takes effect after a DRV.NVSAVE command and after rebooting the AKD.Save the parameters in the non-volatile memory via a DRV.NVSAVE command and turn off/on the 24[V] power supply in order to reboot the drive or restore the original stetting of VBUS.HALFVOLT.None

n151

Not enough distance to move; motion exception.For trapezoidal and customer table motion tasks: The target velocity specified in the motion task cannot be reached via using the selected acceleration and deceleration since the distance to travel is not sufficient.
For a 1:1 profile: The selected acceleration and deceleration will be extended since there is too much distance to travel and the motion task would exceed its maximum allowed velocity.
Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. Check motion task settings and parameters to make sure that the values entered will produce a valid motion task.None

n152

Not enough distance to move; following motion exception.A new motion task activated, when one motion task is already active and the target position specified in the motion task parameters cannot be reached with specified target velocity, acceleration and deceleration parameters. The motion task will directly decelerate to into the target position or ramps down to velocity 0 and start another move to reach target position of the next motion task.Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. Check motion task settings and parameters to make sure that the values entered will produce a valid motion task.None

n153

Velocity limit violation, exceeding max limit.A new target velocity calculated internally due to an exception, and is being limited due to user velocity limit.Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. Check motion task target velocity settings and parameters to make sure that the values entered will not exceed the VL.LIMITP and VL.LIMITN setting.None

n154

Following motion failed; check motion parameters.Activation of the following motion task failed due to incompatible parameters, or motion task does not exist.Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. Check following motion task settings and parameters to make sure that the values entered will produce a valid motion task.None

n156

Target position crossed due to stop command.The motion task crosses the target position after triggering a DRV.STOP command. This situation can happen when processing a change-on-the-fly motion task and triggering a DRV.STOP command close to the target position of the currently running motion task.Activation of any new motion or using of DRV.CLRFAULTS will clear the warning.None

n157

Homing index pulse not found.A homing mode with index detection is activated, and index pulse is not detected while moving across the range determined by the hardware limit switches.Activation of any new motion or using of DRV.CLRFAULTS will clear the warning.None

n158

Homing reference switch not found.A homing mode with reference switch detection is activated and the reference switch is not detected while moving across the range determined by the hardware limit switches.Activation of any new motion or using of DRV.CLRFAULTS will clear the warning.None

n159

Failed to set motion task parametersInvalid motion task parameters assignment. This warning can appear upon an MT.SET command.Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. Check motion task settings and parameters.None

n160

Motion task activation failed.Activation of the motion task failed due to incompatible parameters, or motion task does not exist. This warning can appear upon an MT.MOVE command.Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. Check motion task settings and parameters to make sure that the values entered will produce a valid motion task.None

n161

Homing procedure failed.Homing error observed during the operation of homing procedure.Activation of any new motion or using of DRV.CLRFAULTS will clear the warning.None

n163

MT.NUM exceeds limit.This warning appears with n160. This warning is triggered when you try to trigger a motion task > 128 (such as MT.MOVE 130).Trigger only motion tasks between 0 and 128. Activation of any new motion or using of DRV.CLRFAULTS will clear the warning.None

n164

Motion task is not initialized.This warning appears with n160. This warning is triggered when you try to trigger a non-initialized motion task.Initialize the motion task first before starting the task. Activation of any new motion or using of DRV.CLRFAULTS will clear the warning.None

n165

Motion task target position is out.This warning appears with n160. This warning is triggered when you try to trigger a motion task with an absolute target position outside of the selected modulo range (see also MT.CNTL).Move the absolute target position of the motion task within the modulo range.Activation of any new motion or using of DRV.CLRFAULTS will clear the warning.None

n168

Invalid bit combination in the motion task control word.This warning appears with n160. This warning is triggered when you try to trigger a motion task with an invalid bit combination in the motion task control word (see also MT.CNTL).Correct the MT.CNTL setting for the specific motion task. Activation of any new motion or using of DRV.CLRFAULTS will clear the warning.None

n169

1:1 profile cannot be triggered on the fly.This warning appears with n160. This warning is triggered when you try to trigger a 1:1 profile table motion task while another motion task is currently running.1:1 profile table motion tasks should be started from velocity 0. Activation of any new motion or using of DRV.CLRFAULTS will clear the warning.None

n170

Customer profile table is not initialized.This warning appears with n160. This warning is triggered when you try to trigger a motion task that uses a customer profile table for generating the velocity profile and when the selected profile table is empty (see MT.CNTL and MT.TNUM.Change the MT.TNUM parameter for this specific motion task in order to use an initialized profile table. Activation of any new motion or using of DRV.CLRFAULTS will clear the warning.None

F201

Internal RAM failed.

Hardware failure detected.

Restart drive. If issue persists, contact technical support.

Disable power stage

F202

External RAM failed.

Hardware failure detected.

Restart drive. If issue persists, contact technical support.

Disable power stage

F203

Code Integrity failed.

Software failure detected. FPGA register access failure occurred.

Restart drive. If issue persists, contact technical support.

Disable power stage

F204

Control board EEPROM read failed.

EEPROM failure detected.

Restart drive. If issue persists, exchange drive.

Disable power stage

F205

Control board EEPROM corrupted serial num stamp.

EEPROM failure detected.

Restart drive. If issue persists, exchange drive.

Disable power stage

F206

Control board EEPROM corrupted serial num data.

EEPROM failure detected.

Restart drive. If issue persists, exchange drive.

Disable power stage

F207

Control board EEPROM corrupted parameter stamp.

EEPROM failure detected.

Restart drive. If issue persists, exchange drive.

Disable power stage

F208

Control board EEPROM corrupted parameter data.

EEPROM failure detected.Restart drive. If issue persists, exchange drive.Disable power stage

F209

Power board EEPROM read failed.

EEPROM failure detected.Restart drive. If issue persists, exchange drive.Disable power stage

F210

Power board EEPROM corrupted serial num stamp.

EEPROM failure detected.Restart drive. If issue persists, exchange drive.Disable power stage

F212

Power board EEPROM corrupted serial num data.

EEPROM failure detected.Restart drive. If issue persists, exchange drive.Disable power stage

F213

Power board EEPROM corrupted parameter stamp.

EEPROM failure detected.Restart drive. If issue persists, exchange drive.Disable power stage

F214

Power board EEPROM corrupted parameter data.

EEPROM failure detected.Restart drive. If issue persists, exchange drive.Disable power stage

F219

Control board EEPROM write failed.

EEPROM failure detected.

Restart drive. If issue persists, exchange drive.

Disable power stage

F230

Power board EEPROM write failed.

EEPROM failure detected.

Restart drive. If issue persists, exchange drive.

Disable power stage

F232

Power board EEPROM invalid data.

EEPROM failure detected.

Restart drive. If issue persists, exchange drive.

Disable power stage

F234

n234

Control over temperature sensor 1.

High temperature limit reached.

Check cabinet ventilation system.

Disable power stage

F235

n235

Power over temperature sensor 1.

F236

n236

Power over temperature sensor 2.

F237

n237

Power over temperature sensor 3.

F240

n240

Control under temperature sensor 1.

Low temperature limit reached.

Check cabinet ventilation system.

Disable power stage

F241

n241

Power under temperature sensor 1.

F242

n242

Power under temperature sensor 2.

F243

n243

Power under temperature sensor 3.

F245

External Fault.

This fault is user generated and is caused by user settings.

Users can configure a digital input to trigger this fault (DINx.MODE = 10). The fault occurs according to this input setting. Clear the input to clear the fault.

Disable power stage

F247

Vbus read is out of thresholds.

Hardware problem in bus measurement.Troubleshoot and repair hardware problem.Disable power stage
F248

Option board EEPROM corrupted.

EEPROM failure detected.Restart drive. If issue persists, exchange drive.Disable power stage
F249

Option board downstream checksum.

Communications with the I/O on the option board failed.DRV.CLRFAULTS. If issue persists If issue persists, contact technical support.Disable power stage
F250

Option board upstream checksum.

Communications with the I/O on the option board failed.DRV.CLRFAULTS. If issue persists If issue persists, contact technical support.Disable power stage
F251

Option board watchdog.

Communications with the I/O on the option board failed.DRV.CLRFAULTS. If issue persists If issue persists, contact technical support.Disable power stage
F252

Firmware and option board FPGA types are not compatible.

The option board FPGA is not compatible with this hardware.Download the correct firmware file for this drive.Disable power stage
F253

Firmware and option board FPGA versions are not compatible.

The version of the option board FPGA is not compatible with this firmware.Download the correct firmware file for this drive.Disable power stage
F256Analog Input over voltageThe analog input value is above the AIN.OVFTHRESH level.Check the analog input signal or change the AIN.OVFTHRESH value.Controlled Stop
F257Analog Input under voltageThe analog input value is below the AIN.UVFTHRESH level.Check the analog input signal or change the AIN.UVFTHRESH value.Controlled Stop
n256Warning: Analog Input over voltageThe analog input value is above the AIN.OVWTHRESH level.Check the analog input signal or change the AIN.OVWTHRESH value.None
n257Warning: Analog Input under voltageThe analog input value is below the AIN.UVWTHRESH level.Check the analog input signal or change the AIN.UVWTHRESH value.None

F301

n301

Motor overheated.

Motor overheated.

Check ambient temperature. Check motor mounting heat sink capability

Disable power stage

F302

Over speed.

Motor exceeded VL.THRESH value.

Increase VL.THRESH or lower velocity command.

Dynamic braking

F303

Run away.

Motor did not follow command values.

Current command to the motor is too high for too long. Reduce servo gains, or reduce command trajectory aggressiveness.Controlled stop

F304

n304

Motor Foldback.

Maximum motor power has been exceeded; the power has been limited to protect the motor

Motion is requiring too much power. Change move profile to reduce load on motor. Check for load jamming or sticking. Check that current limits are set correctly.

Controlled stop

F305

Brake open circuit.

Motor brake open circuit. Fault threshold is 200 mA.

Check cabling and general functionality. For special low current brake applications, the F305 fault can be bypassed using the setting motor.brake = 100.

Dynamic braking

F306

Brake short circuit.

Motor brake short circuit.

Check cabling and general functionality. Check that MOTOR.TBRAKERLS and MOTOR.TBRAKEAPP are configured.

Dynamic braking

F307

Brake applied during Enable-State.

Motor brake closed unexpectedly.

Check cabling and general functionality.

Dynamic braking

F308

Voltage exceeds motors rating.

Drive bus voltage exceeds the motor’s defined voltage rating.

Make sure that the motor fits the driving rating.

Disable power stage
n309Motor I2t load. reduce loadMotor I2t load (IL.MI2T) has exceeded the warning threshold IL.MI2TWTHRESH. This warning can only be generated in the case that the motor protection mode IL.MIMODE has been set to 1.Reduce the load of the drive by adjusting lower acceleration / deceleration ramps.None
F312

Brake released when it should be applied.

Brake disengaged unexpectedly.Check cabling and general functionality.Controlled stop

F401

Failed to set feedback type.

Feedback is not connected or wrong feedback type selected

Check primary feedback (X10 connection).

Dynamic braking

F402

Analog signal amplitude fault.

Analog signal amplitude is too low. Analog fault (resolver signal amplitude or sin/cos amplitude)

Check primary feedback (X10 connection), resolver and sine/cos encoder only.

Dynamic braking

F403

EnDat communication fault.

General communication problem with feedback.

Check primary feedback (X10 connection), EnDat only. If feedback is linear, check calibration.

Dynamic braking

F404

Illegal Hall state (111, 000).

Hall sensor returns invalid Hall state (111, 000); either all Hall sensors are on or off. Legal Hall states are 001, 011, 010, 110, 100, and 101. This fault can be caused by a broken connection in any one of the Hall signals.

Check the feedback wiring; check all feedback connectors to ensure all pins are positioned correctly.

Dynamic braking

F405

BiSS watchdog fault.

Bad communication with the feedback device.

 

 

Check primary feedback (X10 connection), Biss only.

Dynamic braking

F406

BiSS multi cycle fault.

F407

BiSS sensor fault.

F408

SFD configuration fault.

Bad communication with the feedback device.

 

 

 

 

 

Internal feedback failure. Return to manufacturer for repair.

Dynamic braking

F409

SFD UART over run fault.

Internal feedback failure. Return to manufacturer for repair.

F410

SFD UART frame fault.

Internal feedback failure. Return to manufacturer for repair.

F412

SFD UART parity fault.

Internal feedback failure. Return to manufacturer for repair.

F413

SFD transfer timeout.

Check primary feedback (X10 connection), SFD only.

n414

SFD single corrupted position.

Internal feedback failure. Return to manufacturer for repair.

F415

SFD multiple CRC error.

General communication problem with feedback (internal feedback failure).

Check primary feedback (X10 connection). Contact manufacturer for repair.

Dynamic braking

F416

SFD transfer incomplete.

General communication problem with feedback (internal feedback failure).

Check primary feedback (X10 connection), SFD only.

Dynamic braking

F417

Broken wire in primary feedback.

In primary feedback, a broken wire was detected (incremental encoder signal amplitude).

Check feedback cable continuity.

Dynamic braking

F418

Primary feedback power supply.

Power supply fault for primary feedback.

Check primary feedback (X10 connection).

Dynamic braking

F419

Encoder init procedure failed.

Phase find procedure did not complete successfully.

Check encoder wiring, reduce/balance motor load prior to phase finding.

Disable power stage
F420

FB3 Endat communication fault.

A communication error was detected with the EnDat 2.2 device connected to the X9 connector.Check pinout and FB3 configuration and reconnect feedback. If problems persist, contact customer support.Dynamic braking
F421

SFD resolver sensor fault.

Sensor or sensor wiring failure inside motor.Try resetting the fault. If it reappears return motor for repair.Dynamic braking
F423

NV Failure – Extended Multiturn.

The position saved in memory is corrupted.Home axis or disable extended multiturn. If the fault persists, send the drive for repair.Disable power stage

F438

n439

Deviation from predicted trajectory fault.

Motor did not follow command values. Motor exceeded maximum allowed position following error (numeric).

Check for increased load, jamming or sticking. Is position error set too low?

Controlled stop

F439

n439

Following error magnitude fault.

Motor did not follow command values.

Motor exceeded maximum allowed position following error (user).

Check feedback commutation setup and tuning parameters.

Controlled stop

F450

Following error presentation.

Motor did not follow command values. Motor exceeded maximum allowed position following error (presentation).

Check feedback commutation setup and tuning parameters.

Controlled stop
F451
n451

Feedback battery fault.

The external battery voltage is too low. The F451 fault is generated if the AKD is not powered. The n451 warning is generated if the AKD is powered. This fault can be inhibited with FAULT451.ACTION.Check or replace the external battery.Dynamic braking
F452Extended Multiturn not supported with this feedback.Non-multiturn feedback is connected while FB1.PMTSAVEEN is active.Connect multiturn feedback to the drive or disable extended multiturn.Disable power stage
F453Tamagawa communication fault (timeout).Bad communication with the feedback device. Cabling or shielding fault, or internal feedback failure.Check the cabling to the drive and if the problem persists then return the feedback to the manufacturer for repair.Dynamic braking
F454Tamagawa communication fault (transfer incomplete).
F456Tamagawa communication fault (CRC).
F457Tamagawa communication fault (start timeout).
F458Tamagawa communication fault (UART Overrun).
F459Tamagawa communication fault (UART Framing).
F460Tamagawa encoder fault (over speed).This fault is generated when the shaft is rotated above a maximum speed that can be maintained while the external battery is powered and the drive is powered off.Reset the fault on the drive with DRV.CLRFAULTS.Dynamic braking
F461Tamagawa encoder fault (counting Error).When the feedback is powered on the position (within one revolution) was incorrect because of a problem with the feedback device.Reset the fault on the drive with DRV.CLRFAULTS, if the problem persists then clean the feedback code plate.Dynamic braking
F462Tamagawa encoder fault (counting overflow).Multi-turn counter has overflowed.Reset the fault on the drive with DRV.CLRFAULTS.Dynamic braking
F463Feedback overheat fault.The temperature of the encoder substrate exceeds overheating detection temperature during main power-on.Reset the fault on the drive with DRV.CLRFAULTS after temperature of encoder is lowered.Dynamic braking
F464Tamagawa encoder fault (multi-turn error).Any bit-jump occurs in the multi-turn signal during main power-on.Return to the origin. Reset the fault on the drive with DRV.CLRFAULTS.Dynamic braking
F465Excessive shock detected by feedback device.

1. Excessive shock from an impact or vibration has caused an error in the feddback device.

or

2. Internal error in the feedback device mechanism, resulted in bad position data.

1. Reduce external impacts to the motor housing and shaft. Tune the control loops filters. Reduce gains, particularly feed forward gains. Reduce maximum commanded acceleration.

or

2. Replace the feedback device.

Dynamic braking
F467Feedback fault on feedback 1 (See FB1.FAULTS for details).The feedback device malfunctioned.

Check FB1.FAULTS for detailed fault information.

If using a BiSS feedback device, fault 467 indicates a communications fault with the BiSS feedback device. No additional information is available via FB1.FAULTS for this fault when using a BiSS feedback device.

Dynamic braking
F469FB1.ENCRES is not power of two, Remote Commutation not possible.Feedback Type 43 requires that the feedback resolution be a power of two. Feedback Type 43 is not supported for all feedback resolutions.If the remote feedback device's resolution is a power of two, enter that value in FB1.ENCRES. Otherwise, choose a feedback device with a supported resolution (power of two) and enter that value in FB1.ENCRES.Dynamic braking
F470Feedback fault on feedback 3.Feedback is not connected or general communication problem.Check tertiary feedback (X9 connection)Dynamic braking

F473

Wake and Shake - Insufficient movement

There was less movement than defined by WS.DISTMIN.

Increase WS.IMAX and/or WS.T. Or try using WS.MODE 1 or 2.

Disable power stage

F475

Wake and Shake - Excess movement

WS.DISTMAX has been exceeded in WS.MODE 0. Or more than 360 degrees was traveled in WS.MODE 2.

Increase WS.DISTMAX value or reduce WS.IMAX or WS.T. Wake and Shake is not suported for vertical/overhung loads.

Disable power stage

F476

Wake and Shake - Fine-Coarse delta too large.

The angle difference between the coarse and fine calculation was larger than 72 deg.

Modify WS.IMAX or WS.T and try again.

Disable power stage

F478

n478

Wake and Shake - Over speed

WS.VTHRESH was exceeded.

Increase WS.VTHRESH value or reduce WS.IMAX or WS.T.

Disable power stage

F479

n479

Wake and Shake - Loop angle delta too large.

The angle between complete loops was larger than 72 deg.

Modify WS.IMAX or WS.T and try again.

Disable power stage

F480

Field bus command velocity too high.Fieldbus command velocity exceeds VL.LIMITP.Lower fieldbus command trajectory, or increase the value of VL.LIMITP.Disable power stage

F481

Field bus command velocity too low.Fieldbus command velocity exceeds VL.LIMITN.Increase fieldbus command trajectory, or decrease the value of VL.LIMITN.Disable power stage

F482

Wake and Shake - Commutation not initialized.The motor requires the commutation initialization (there are no encoder commutation tracks, Hall sensors, etc.) and no successful Wake and Shake sequence has been performedClear any faults, activate the Wake and Shake procedure (WS.ARM) and enable the drive.Disable power stage

F483

Wake and Shake - Motor U phase missing.No current was detected in the motor's U phase during Wake and Shake initialization (Mode 0 only).Check the motor connections and WS.IMAX (very low current may produce this error).Disable power stage

F484

Wake and Shake - Motor V phase missing.No current was detected in the motor's V phase during Wake and Shake initialization (Mode 0 only).Check the motor connections and WS.IMAX (very low current may produce this error).Disable power stage

F485

Wake and Shake - Motor W phase missing.No current was detected in the motor's W phase during Wake and Shake initialization (Mode 0 only).Check the motor connections and WS.IMAX (very low current may produce this error).Disable power stage
F486Input change rate exceeds maximum speed of emulated encoder.Motor velocity exceeds the maximum speed the emulated encoder output can generate.Reduce value of DRV.EMUEPULSEWIDTH.Controlled stop
F487Wake and Shake - Validating Positive Movement Failed.After applying a positive current, motor moved in the wrong direction.Check motor phase wiring and motor encoder wiring is correct.Disable power stage
F489Wake and Shake - Validating Negative Movement Failed.After applying a negative current, motor moved in the wrong direction.Check motor phase wiring and motor encoder wiring is correct.Disable power stage
F490Wake and Shake - Validating Comm. angle timed out.During one of the W&S validation stages, the drive stopped responding to commands.Contact customer support.Disable power stage
F491Wake and Shake - Validating Comm. angle moved too far - Bad Comm Angle.After applying a current, the motor moved too far (>15 electrical degrees).This indicates a poor motor phase angle was found by Wake and Shake. Revise Wake and Shake parameters, and re-run Wake and Shake.Disable power stage
F492Wake and Shake - Validating Comm. angle required more than MOTOR.ICONTA current larger than MOTOR.ICONT was used to excite the motor.

This indicates one of the following:

  1. Phase angle is incorrect due to a bad wake and shake.
  2. Motor has very high friction requiring high current to break free.
  3. Motor power cable is disconnected or improperly wired.
Disable power stage
F493Invalid commutation detected - motor accelerating in the wrong direction. Motor phase may be incorrect.The velocity of the motor exceeded WS.CHECKV and the sign of the current was not equal to the sign of motor acceleration or the sign of motor velocity for a period of time larger than WS.CHECKT.

1. Check motor phase wiring

2. Re-configure wake and shake (if Mode 0 or 1 is used)

3. Re-run wake and shake to determine correct commutation angle

Dynamic braking

F501

n501

Bus over voltage.

Bus voltage too high. Usually, this problem is load related.

Reduce load or change motion profile. Check system regen capacity; add capacity if needed. Check mains voltage.

Disable power stage

F502

Bus under voltage.

Warning issued prior to fault.

Bus voltage below threshold value.

Check mains voltage.

Controlled stop

F503

n503

Bus capacitor overloaded.

Single phase AC input on a drive only rated for three-phase input or excessive single-phase power load.

Check mains voltage.

Controlled stop

F504

1V2 over voltage.

Internal supply voltage fault detected.

Check wiring for electromagnetic compatibility (EMC). If issue persists exchange drive.

 

 

 

 

Controlled stop

F505

1V2 under voltage.

F506

2V5 over voltage.

F507

2V5 under voltage.

F508

3V3 over voltage.

F509

3V3 under voltage.

F510

5V0 over voltage.

F512

5V0 under voltage.

F513

+12V0 over voltage.

F514

+12V0 under voltage.

F515

-12V0 over voltage.

F516

-12V0 under voltage.

F517

Analog 3V3 over voltage.

F518

Analog 3V3 under voltage.

F519

Regen short circuit.

Regen resistor short circuit.

Regen IGBT short circuit. Contact technical support.

Disable power stage

F521

n521

Regen over power.

 

Too much power stored in regen resistor.

Either get larger regen resistor or use DC bus sharing to dissipate power.

Disable power stage

F523

Bus over voltage FPGA.

Bus over voltage hard fault.

Check mains voltage and check system brake capacity.

Disable power stage

F524

n524

Drive Foldback.

Maximum drive power has been exceeded. The power has been limited to protect the drive.

Motion requires too much power. Change profile to reduce load .

Controlled stop

F525

Output over current.

Current exceeds drive peak.

Check for short or feedback faults.  

Disable power stage

F526

Current sensor short circuit.

1. Current sensor short circuit.

2. Motor cable plugged in upside down

1. Restart drive. If issue persists, contact technical support.

2. Plug in cable right-side up.

Disable power stage

F527

Iu current AD converter stuck.

Hardware failure detected.

Restart drive. If issue persists, contact technical support.

Disable power stage

F528

Iv current AD converter stuck.

Hardware failure detected.

Restart drive. If issue persists, contact technical support.

Disable power stage

F529

Iu current offset limit exceeded.

Hardware failure detected.

Restart drive. If issue persists, contact technical support.

Disable power stage

F530

Iv current offset limit exceeded.

Hardware failure detected.

Restart drive. If issue persists, contact technical support.

Disable power stage

F531

Power stage fault.

Hardware failure detected.

Restart drive. If issue persists, replace drive.

Disable power stage

F532

Drive motor parameters setup incomplete.

Before a motor can be enabled, you must configure a minimum set of parameters. These parameters have not been configured.

Issue the command DRV.SETUPREQLIST to display the list of the parameters that you must configure. Configure these parameters either manually or automatically. You can manually configure these parameters in three ways: (1) set each parameter individually; (2) use the setup wizard to select the motor; or (3) select the motor type from the motor data base in the Motor window (MOTOR.AUTOSET must be set to 0 (off)). If you use the Motor window, you must first select the feedback type. If the motor has Biss Analog, Endat, or SFD feedback (feedback with memory), then these parameters are set automatically when MOTOR.AUTOSET is set to 1 (on).

Disable power stage

F534

Failed to read motor parameters from feedback device.

Motor either does not have motor feedback memory, or the motor feedback memory is not programmed properly so the parameters cannot be read.

Try to read parameters again by clicking the Disable and Clear Faults button, or by issuing the DRV.CLRFAULTS command. If this attempt is not successful, then set MOTOR.AUTOSET to 0 (off) and program the parameters using the setup wizard or manually set up the parameters. If the motor has motor memory (Biss Analog, Endat, and SFD motors have motor memory), return the motor to have the memory programmed.

Dynamic braking
F535Power-board over-temperature fault.The power-board temperature sensor indicates more than 85 °C.Reduce the load of the drive or ensure better cooling.Disable power stage
F536Standby power supply fault.Standby voltage circuit overloaded.Check total 24 V power load of AKD-N in the strings (sum of drive and motor brake supply). The AKD-C must be power-cycled to recover from this fault.Disable Drives
F537Precharge fault.Precharge process could not be performed in a reasonable amount of time.Look for a shortcut in the string (cable) or exchange hardwareDisable Drives and Unpower Strings
F541AC input phase 1 missing.Mains supply failure detected, phase L1 missed.Check power connector and power source.Disable Drives and Unpower Strings
F542AC input phase 2 missing.Mains supply failure detected, phase L2 missed.Check power connector and power source.Disable Drives and Unpower Strings
F543AC input phase 3 missing.Mains supply failure detected, phase L3 missed.Check power connector and power source.Disable Drives and Unpower Strings
F545String current over peak limitString current is higher than AKD-C Rated Peak Current.Lower AKD-N current limits to prevent overdrawing AKD-C currentDisable Drives and Unpower Strings
F546String current over continuous limitString current is higher than AKD-C Rated Continuous Current (I²T).Lower AKD-N current limits to prevent overdrawing AKD-C currentDisable Drives and Unpower Strings
F560Regen near capacity, could not prevent over voltage.An F501 Bus Over Voltage has occured while the Regen Resistor was at or above 75% of its dissipation capacity.Increase the size of regen resistor to be able to dissipate more power.Disable power stage
F561More than 8 AKD-Ns connected at string2Too many drives on string 2.Reduce NSDs on String 2 to 8 or lessDisable Drives and Unpower Strings
F562More than 8 AKD-Ns connected at string1Too many drives on string 1.Reduce NSDs on String 1 to 8 or lessDisable Drives and Unpower Strings
F564Number of connected nodes on string 1 has decreased.Drive has been removed from string 1.Investigate AKD-N Ethercat communication, determine where network connection failed.Disable Drives and Unpower Strings
F565Number of connected nodes on string 2 has decreased.Drive has been removed from string 2.Investigate AKD-N Ethercat communication, determine where network connection failed.Disable Drives and Unpower Strings
F570Phase loss.Phase loss detected.Check mains power voltage. Fault action configurable by FAULT570.ACTION.Disable power stage
n582Velocity has been limited commutation speed to less than 600Hz to meet ECCN 3A225 requirements.Motor Velocity has exceeded the allowed commutation speed (599Hz).Refer to ECCN 3A225 Limitations for Induction Motors.Velocity command will be clamped at ECCN 3A225 regulation.
n601Modbus data rate is too high.Modbus controller data rate is too high.Reduce data rate.Disable power stage

F602

Safe torque off.

Safe torque off function has been triggered.

Reapply supply voltage to STO if safe to do so.

Disable power stage
n603OPMODE incompatible with CMDSOURCEThis warning is generated when the drive is enabled and the gearing command source is selected at the same time as torque or velocity op-mode.Select a different DRV.OPMODE andDRV.CMDSOURCE combination.Disable power stage
n604EMUEMODE incompatible with DRV.HANDWHEELSRC.Emulated encode mode is incompatible with the selected handwheel source.Select a compatible emulated encode mode or change handwheel source.Disable power stage
F621Control Board CRC fault.Communications with the Power Board FailedDRV.CLRFAULTS. If issue persists, contact technical support.Disable power stage
F623Power Board CRC fault.
F624Power Board Watchdog fault.
F625Power Board Communication fault.
F626Power Board FPGA not configured.
F627Control Board Watchdog fault.
F628AKD-C Front door packet not received on String 1.A data packet has not been received by the AKD-N or AKD-C (String 1)Check cables and clear the fault.Disable Drives and Unpower Strings
F629AKD-C Front door packet not received on String 2.A data packet has not been received by the AKD-C (String 2)Check cables and clear the fault.Disable Drives and Unpower Strings

F630

FPGA cyclic read fault.

FPGA-to-firmware data access error.

DRV.CLRFAULTS. If issue persists, contact technical support.

Disable Power Stage

F701

Fieldbus Runtime.

Runtime communication fault.

Check fieldbus connections (X11), settings, and control unit.

Controlled stop

F702

n702

Fieldbus Communication lost.

 

All fieldbus communication was lost.

Check fieldbus connections (X11), settings, and control unit.

Controlled stop

F703

Emergency timeout occurred.

Motor did not stop in the timeout defined.

Change timeout value, change stop parameters, improve tuning.

Disable power stage

About this Article

Kollmorgen Support