Skip to main content

Kollmorgen Support Network

AKD CoE Interpolated Position Mapping | 03 Aug 2016 | |

AKD CoE Interpolated Position Mapping

I have attached two screen shots of typical CoE (CanOpen over EtherCAT) mapping for position control using 0x6060 Interpolated position mode (7).  scale is set by FBUS.PSCALE in units of the power of 2.  Default is 2^20 counts/rev of the motor.

About this Article

Kollmorgen Support