The AKD command source (DRV.CMDSOURCE) is set automatically by the EtherCAT/CANopen master controller. There is no need to set this in Workbench when using the fieldbus. And there is no need to read DRV.CMDSOURCE to verify that it's set correctly…
Raspberry Pi Foundation and its background.
The foundation's goal was to advance the Computer Science, Programming, and engineering education of children and adults with a low-cost and high-performance solution.
From Raspberry Pi Foundation itself:
The ability to read FB3.P was added in firmware 01-12-00-000.
This application note demonstrates configuration, key objects, and reading the encoder position using both PCAN
for CANopen and TwinCAT3 for EtherCAT.
Help setup the AKD2G in DS402 Profile Velocity mode.
This document assumes the EtherCAT Master has “free mapping” function available. The ability to select what data is to be shard every update cycle. This information may not make sense to you but…