Skip to main content

Kollmorgen Support Network

Switch On Sequence | 11 Apr 2011 | |

Switch On Sequence

Valid for S300, S700

General

The behavior of the servo amplifier always depends on the current setting of a number of different parameters (e.g. ACTFAULT, VBUSMIN, VELO, STOPMODE etc.).

The built-in safety function STO can be used to switch off the drive, so that personnel safety is ensured at the drive shaft.

In case of a built-in safety card in the S700, please check the "Ready Acknowledge" (X30 Pin 16) signal before enabling the servo amplifier. An error would occur, if you enable the servo amplifier without ready to operate safety card.

The diagrams below illustrate examples for the correct functional sequence for switching the servo amplifier on and off.

Without holding brake

Switch on and switch off behavior:

With holding brake

Devices which are equipped with a selected (holding- ) "Brake" function use a special sequence for switching off the output stage.
This is an example for S700:

 

About this Article

Kollmorgen Support