Skip to main content

Kollmorgen Support Network

Expansion Card PROFIBUS-DP | 29 Oct 2010 | |

Expansion Card PROFIBUS-DP

Usable with S300, S700

General

This expansion card can be used with S300 and S700.
The PROFIBUS Bus expansion card has two 9-pin SubD sockets wired in parallel.
Function blocs for S7 PLC from Siemens and manufacturer independant PLCs are available from the Downloads page.

The command OPTION delivers a code for the built-in expansion card.

Expansion card

Front cover

Setup

Station address and Baud Rate

  • keypad on the front panel of the servo amplifier
  • setup software: screen page “CAN / Fieldbus"
  • serial interface with a sequence of ASCII commands:
    ADDR => SAVE => COLDSTART (with nn = address)

Documentation

Data sheets for the expansion card can be found via File Selector, set document type filter to "Add On Document".

Back to top

About this Article

Kollmorgen Support