Writing Data to the PDMM SD Card or Embedded Flash
This application note describes the process of writing data to the SD card or the embedded flash on the PDMM in .CSV (comma separated variable) format. This is a general overview for writing data. More read/write functions can be found in the KAS help section under File Management Functions.
Write Data to SD Card
Data logging with an SD card is used when a user wants to collect data from the PDMM, and then view this data on another computer.
Mount the SD card (Step 1)
Before any data transaction can take place, the SD card must be mounted. To accomplish this, you would use the SD_MOUNT() instruction. This instruction must be executed when a KAS program is running. I would suggest executing SD_MOUNT() in a startup routine.

Note: if you wish to remove the SD card you must first use SD_UNMOUNT() instruction to avoid file corruption.
Obtain a File ID (Step 2)
To obtain a File ID, you will need to use the F_AOPEN or F_WOPEN instruction (see File Management Functions in KAS help section for the difference between these 2 instructions). These functions will return a DINT as a File ID.
This instruction takes a string in as an argument. This string should be the name of the file you wish to write to with a prefix of //SDCard/. This file should have an extension of .csv.

Write Data String (Step 3)
To write data to the SD you will need to do 2 things:
- Build a string with all the data needed to log, with a comma in between each piece of data
- Use a FM_WRITE instruction
To build a string, you need to use the CONCAT function. Once you build your string, you can write to the SD card with the file ID.

Note: Upon completion of the FM_WRITE instruction, it will return a bool value. This value will be true if the instruction wrote the data, and false if it did not. It is a good suggestion to use this return value to implement error handling.
View Data (Step 4)
Remove the SD card from the PDMM and insert into SD reader. Warning! You must “unmount” the SD card before removing.
Entire Example Program (Step 5)

Write Data to Embedded Flash
Data logging to the PDMM embedded flash memory can be used if the user does not have an SD card or is simply always connected to the system.
Logging to embedded flash is very similar to the SD card, except you do not need to mount the SD and you do not need the //SDCard/ prefix on the file name.
- Obtain a File ID
To obtain a File ID, you will need to use the F_AOPEN or F_WOPEN instruction (see File Management Functions in KAS help section for the difference between these 2 instructions). These functions will return a DINT as a File ID.

- Write Data String
This is the same as writing to the SD card. Refer to step 3 in the Write Data to SD Card
- View Data
From your computer open the IE browser and type in the PDMM IP address. Go to the User Data tab in the webserver. Right click on the file and either open or save file to computer (see image below).

- Entire Example Program

Home >
Knowledge Base >
FAQs >
Downloads >