Ana içeriğe atla

Search Articles

KAS project EtherCAT mapping - S700 Dig InputsThe following outlines setting up KAS project to read S700 Digital Inputs into a PxMM program: Through high speed , deterministic PDO channel: Use S700 FW 5.18 or greater İngilizce
Scoping the Resolver or Sine Encoder Signal Amplitude in AKDFirst to review what F402 means: Analog signal amplitude for resolver or sine encoder feedback is out of range, either too low or too high. To troubleshoot: Check primary feedback (X10 connection), for resolver and sine/cos encoder only. İngilizce
Frameless Motor Mounting Practices: Clamping and BoltingEmbedded Motion Technology - Frameless  Mounting Considerations The benefits of Improved System Performance, Reduced Maintenance, Smaller Mechanical Footprint, Higher System Efficiency are understood Customer still has a key question in mind …   İngilizce
Frameless Motor Mounting Practices: Bonding with Structural AdhesivesEmbedded Motion Technology - Frameless  Mounting Considerations The benefits of Improved System Performance, Reduced Maintenance, Smaller Mechanical Footprint, Higher System Efficiency are understood Customer still has a key question in mind …   İngilizce
Reading a Drive Parameter with AKD EtherNet/IPThis application note covers the different methods for reading a drive parameter over AKD EtherNet/IP. İngilizce
Home and Latch conflictValid for S400, S600 Problem On a machine the homing procedure NREF 5 (move to the next zero-mark of the feedback unit) is started cyclic.  İngilizce
KAS Controller Error SubprogramsAttached are two subprograms that can be imported to the Project Explorer of the KAS IDE software. İngilizce
Understanding AKD MT LOAD and MT SET Understanding the MT.LOAD and MT.SET command parameters I see this come up a lot and often there is confusion of how these keywords work and what they do. İngilizce
Methods to Configure, Backup, and Restore a PxMM SystemAttached is a word doc: - With a table showing the methods to configure, backup, and restore a PxMM System - Supporting screen shots İngilizce