Ana içeriğe atla

Search Articles

Superior Step Motor Catalog 2006This catalog covers the KM06, KM09, KM11, MH172, MX09, and MX11 series step motors. İngilizce
KAS Associated Firmware By ReleaseThe following table provides a resource for what firmware is associated with each release of the KAS IDE. This includes both firmware for the drive built into the AKD-PDMM controller, as well as the firmware for other drives that may be used within KAS. İngilizce
Ingress Protection of Servo MotorsSealing is an important design tool used to prolong the life of motors against harsh environments containing dust or liquid contaminants. There are arguably an unlimited number of applications for servo motors and each comes with its own environmental challenges. Sealing can be compromised or… İngilizce
Osciloscópio - PDMMNesse artigo abordaremos sobre como utilizar o osciloscópio presente no KAS e como realizar medições em posicionamentos. Portuguese, Brazil
Using a DC Power Supply for AKD Bus PowerMany servo applications exist in which it is more practical to use a DC power supply for the motor bus power instead of using AC power.  Some of these include the use of batteries, generators, low voltage DC power supplies, and there are cases where high voltage DC power supplies are used ju İngilizce
AKD + AKI via ModbusNesse artigo explicamos sobre um projeto que utiliza a comunicação modbus para ligar o AKD a IHM AKI. Portuguese, Brazil
How To Resolve Potential Issues When Importing Data Types for AKD-P EtherNet/IPThis article demonstrates potential issues seen when users attempt to import the data types that the AOIs are codependent on and how to resolve them. İngilizce
Encoder externo (AKD + CODESYS)Esse tutorial mostra como ler a posição do encoder auxiliar conectado no AKD no conector X7/X9, através do protocólo EtherCAT no CODESYS. Abordaremos como adicionar o PDO correspondente e como mapear uma variável para manipular esse dado no… Portuguese, Brazil
Qt pre-built packagePre-built package of Qt, used by KAS development. Redistributed here to be in compliance with the LGPL3 license. İngilizce