IDC B8961/B8962 Commutation Sensor FaultThe 0x0688 or 0x0288 or 0x0289 fault is displayed on the keypad as an Undefined Fault. This fault code will be at the bottom of the keypad display. When connected to the ServoTuner software, these come up as Commutation Sensor Fault errors.
İngilizce
S700 Servo Pump Application NoteTogether with the servo pump functionality, an S700 servo amplifier can be used to power a hydraulic cylinder. The entire system usually consists of a servo amplifier, a motor with position feedback unit, and a hydraulic cylinder with pressure feedback unit. The cascaded pressure/volume regulation…
İngilizce
S700 Servo Pumpe ApplikationsschriftIn Verbindung mit der Servopumpen-Funktionalität, kann ein S700-Servoregler genutzt werden, um einen Hydraulikzylinder anzutreiben. Das Gesamtsystem besteht in der Regel aus einem Servoregler, einem Motor mit Position-Rückführeinheit sowie einem Hydraulikzylinder mit Druck-Rückführeinheit. Die…
Almanca
Hypertherm vertical axis setup issueHypertherm is a CNC for laser/plasma cutting machines. Below are some tips for setting up the AKD drive for use with a Hypertherm machine.
Modbus TCP to AKD BASIC program variables Quick Start Part 1: Modbus PollThis application note serves as a quick start with simple example using a Modbus Master simulator software called Modbus Poll to read/write over Modbus TCP to/from the AKD BASIC program ( variables ). This is part 1 of a two part series.
Boot Time of AKD / AKD2GThe boot time was measured from the point of applying 24V control power to the drives. The time was measured to specific indicators and functions of the drives.
Note that AC power was already turned on prior to running these tests, so that the drives could automatically enable. …