Communicating with the AKD over Telnet using HyperTerminal and PuTTYNormally, the Workbench software is used to connect to and configure the AKD drives. However, there may be some instances where Workbench can't be used or where another communication method is preferred for troubleshooting purposes, etc. Two terminal programs t
AKM Motor Set up for SC900An AKM motor with resolver can be operated with an SC900 series amplifier providing that the motor is within the current limitations of the drive. Typically the motor resolver offset must be set to 240. This is in the configuration screen and called COMMOFF.
AKD Spring Clamp ConnectorsAll Revision 9 and almost all Revision 7 AKD Control boards use Amphenol 3.5mm connectors for X7 and X8.
Both the header and the mating connector are bespoke items from Amphenol. Phoenix numbers for spring clamp connectors are:
AKD Maximum Commutation FrequencyMaximum FW commanded speed is 15,000 RPM.
Maximum commutation frequency is set by PWM frequency and/or position feedback device sampling frequency.
İngilizce
Insulation MaterialInsulation material typically depends upon the application. For example, environmental conditions such as temperature, chemical exposure, and abrasion/tear resistance should all be considered when choosing an insulation material.