Salta al contenuto principale

Kollmorgen Support Network

Search Articles

OPC UA Server with AKI HMI and KVB softwareA video goes through the steps to setup communication between an OPC UA server and an AKI HMI panel using KVB software. Inglese
AKD and S700 Vibration SpecificationsThe AKD Installation Manual, the S700 (S701-S724) Installation Manual, and the S700 (S748-S772) Installation Manual all show a vibration specification as "CLASS 3M1 According To IEC60721-3-3". Inglese
G&L Modbus Serial Example Rev. A 6-3-2019This application note demonstrates specifically with Digital MMC Smartdrive with Drive Resident Control Card to Modbus Poll and to KVB/AKI configured as Modbus Serial masters. Inglese
G&L Modbus TCP ExampleThis application note demonstrates specifically with Digital MMC Smartdrive with Drive Resident Control Card to Modbus Poll and to KVB/AKI configured as Modbus TCP masters. Inglese
Superior Step Motor Catalog 2006This catalog covers the KM06, KM09, KM11, MH172, MX09, and MX11 series step motors. Inglese
KAS Associated Firmware By ReleaseThe following table provides a resource for what firmware is associated with each release of the KAS IDE. This includes both firmware for the drive built into the AKD-PDMM controller, as well as the firmware for other drives that may be used within KAS. Inglese
Ingress Protection of Servo MotorsSealing is an important design tool used to prolong the life of motors against harsh environments containing dust or liquid contaminants. There are arguably an unlimited number of applications for servo motors and each comes with its own environmental challenges. Sealing can be compromised or… Inglese
How To Guide for Migrating from Old Exter/Cimrex panels with G&L drive resident control to KVB.Important to note is that the Import Project feature in KVB is for Exter panel based Information Designer project migration to KVB.  If the HMI project was done with Cimrex panels the migration is two stepped where you need to Inglese
Osciloscópio - PDMMNesse artigo abordaremos sobre como utilizar o osciloscópio presente no KAS e como realizar medições em posicionamentos. Portoghese