OPC UA Server with AKI HMI and KVB software
This video goes through the steps to setup communication between an OPC UA server and an AKI HMI panel using KVB software.
You will:
- Have to go to the Tag setup screen to add another "controller" to the project which, in this case, is the OPC UA server.
- Need to know the URL address where the OPC Server is running, and can setup a login user name and password if it does not support an anonymous login.
You can setup a default name space number which will make entering the names of tags easier.
On the main Tag setup screen, there is a new column to add the string-based names of the variables you want to share with the OPC server.
Loading
Home >
Knowledge Base >
FAQs >
Downloads >