No name would have been more desirable. With the Packman 200, Opteq Robotics has developed a self-driving solution for material flows which makes its way quickly and directly through the aisles to reach its destination, just like the popular arcade…
AKD-N decentralized drives and CDDR motors by Kollmorgen are the core of the innovative OMET Xflex X5, a printing solution with the best returns on investment in terms of market result of narrow web printing of labels and flexible packaging.
PACKAGING DECENTRALIZED SOLUTION AKD N DRIVES AND AKM MOTORS FOR DIRECT MAILING AN EXCELLENT PRESS MAILING SERVICE Decentralizing the system to reduce space and materials Promotional postcards and flyers, membership cards, coupons
Traditional injections molding machines use fixed-speed, three-phase motors that run continuously to drive the hydraulic pumps that power the machine. Excess hydraulic oil, which is especially generated during the “clamp hold” and “cooling” portion…
Known for manufacturing paper bags, laminating and flexo-printing machines, Nort Makina has designed and developed a new paper bag-manufacturing machin. Developed using standard technology, as well as specialised technology, the machine has a minimum…
Challenge: Simplify the candy machine without sacrificing performance.Solution: Couple the AKD® PDMM with the KBM™ series motor to reduce the bill of materials.
Challenge: Simplify machine design and reduce cost without sacrificing performance.Solution: AKD® PDMM based control system consisting of permanent magnet servo motors as well as induction motors with both open and closed loop functionality.
In search of new controllers for register control of a rotogravure printing press, Prinovis Itzehoe GmbH implemented a new motion control solution from Kollmorgen that produced important, measurable results.
Challenge: Increase longevity of motor under high pressure washdowns and maintain cleanliness. Solution: Engineered sealed stainless steel motor and gearbox featuring feedback and power cables.
Formula One racing teams demand the highest performance from every single component, which is why motion system specialist Ball Racing Developments Ltd uses high quality parts supplied by Kollmorgen.