Skip to main content
Success Story | 2 minute read

Magnetic field instead of feed rollers

tecodrive is developing a revolutionary process for material feed applications with the help of servo drives from Kollmorgen

Kollmorgen CA TecoDrive Servo Drive S700 EN fleXfeed

tecodrive GmbH from Garbsen has named its invention "fleXfeed" – and is breaking revolutionary new ground in material feed applications used for metal processing. Thanks to an ingenious magnetic field, "fleXfeed" works on a completely contact-free basis and is much faster than conventional feed rollers. The young company is basing its new solution on the principle of linear direct drive technology. As a partner for the delivery of drive control solutions, Kollmorgen was closely involved at the development stage. The S700 servo drive play a key role in the contact-free feed process.

No terminals or rolling, but really high speeds combined with low operating costs: these few words pretty much encapsulate the benefits of the feed device from tecodrive. tecodrive is a successful "spin-off" from the Institut für Umformtechnik und Umformmaschinen (Institute for Forming Technology and Forming Machines) at Leibniz Universität Hannover (Leibniz University, Hanover). The potential of this invention becomes clear if you take a look at sheet metal processing. The lighting experts at TriluX in Arnsberg punch reflector plates for high-end lighting systems out of thin aluminum. Previously, the punch worked with a conventional feed roller at a rate of 200 strokes per minute. A higher cycle rate was not possible. The limiting factor was not the actual punch, however, which could easily have managed double the rate. The problem was due to "the feed roller limiting productivity", as Dr. Olaf Marthiens explains, a managing partner at tecodrive GmbH. The "speed limit" associated with feed roller applications can be explained in terms of physical causes, particularly mass inertia and the coefficient of friction between the strip and the rollers. Kollmorgen CA TecoDrive Servo Drive S700 EN The contact-free technology conveys material into systems really smoothly and at very high speeds, without any transverse forces and without any kinks forming in the strip. Volkswagen in Hanover has been an enthusiastic adopter of this new technology and has managed to reduce setup, maintenance, and stoppage times significantly during the production of filigree radiator fins.

No torsion or slipping
Anyone keen to reap the full benefits of the electromagnetic solution would do well to take a cursory look at how a feed roller works. This positions a strip of metal (rolled out from a coil) and feeds it at a given rate into a machine to be processed – for example, a system for deep drawing or punching. The two rollers must close in with each cycle, building up pressure on the workpiece and transporting it as they jam against it, before finally opening again (or releasing). "The higher the speed, the higher the pressure needs to be so the material does not slip," explains Marthiens. And this is precisely where feed rollers are at a disadvantage compared with the electromagnetic approach. The pressing force exerted on the material cannot simply be increased ad infinitum, or the metal will become deformed. There is also an increased risk that finely worked surfaces may become damaged. TriluX found that this effect was creating torsion – albeit barely visible – in the aluminum fins. Following final assembly, however, this regularly caused noticeable distortion in the light generated.

These days, the lighting manufacturer is using the "fleXfeed" from tecodrive – with astonishing results. The company has doubled its production rate and is now finally able to exploit the full potential of its sheet metal processing machines. "Our mission at the start of the project was to reach 400 strokes a minute – and we achieved this really easily," recalls Hans-Jörg Lindner, who is also a managing partner at tecodrive. "Generally speaking, we are managing to ramp up existing processes by a factor of two," adds Dr. Marthiens.

Kollmorgen CA TecoDrive Servo Drive S700 EN Schematic representation Where does this performance come from? As with linear direct drive technology, the contact-free feed process also adopts the principle of magnetic attraction and repulsion. This explains why the device, at just short of 1 m long, contains two opposing stators. These generate a traveling magnetic wave in the metal strip lying between them, a wave which facilitates the feed action via the Lorentz force generated. The operating principle in the "fleXfeed" could be compared with an asynchronous linear drive, with the metal sheet assuming the role of the squirrel-cage rotor. This detail presents certain challenges from a control technology perspective, however, and the patented process is ultimately concerned with addressing these.

Developing a new control process
Kollmorgen CA TecoDrive Servo Drive S700 EN S700This is where tecodrive relies on the great performance of Kollmorgen's S700 servo drives – particularly in terms of speed and programmability. Maximum freedom is what Dr. Olaf Marthiens needed to implement a new type of control in the servo inverters, an alternative to field-oriented vector control (FOC). "I had to write a program that allows me to change both the phase angle of the current and the amplitude." Using FOC would not really work for this specific application, because the constantly changing magnetic behavior of the material being transported would make the control circuit unstable. FOC would react with great sensitivity to the so-called rotor constant – the ratio between inductance and electric resistance in the sheet metal being conveyed. In a standard asynchronous motor, the rotor is mechanically unchanged and the rotor constant is only dependent on the temperature. Even this can be enough to make an applicator white hot when using asynchronous motors in highly dynamic control applications.

By contrast, the "fleXfeed" unit is designed to position and feed the widest possible range of metal materials into a processing machine with real accuracy in highly dynamic applications. Here too, the different thicknesses and widths and the invisible changes in the structure of the material result in ever-changing resistance and inductance levels – and therefore changes in rotor constants.

Together with Kollmorgen, tecodrive has solved this problem by only having one current and position controller in this particular application. Field-oriented control no longer applies, because the S772 servo inverter is programmed to specify and fix the field. "Our special expertise comes into play here," enthuses Marthiens. In order to determine the position of the sheet metal,tecodrive uses measuring wheels developed in-house for feedback purposes. What's remarkable is the speed of the control circuit, because tecodrive calculates the next set point directly from the actual position of the sheet metal within the magnetic field – and not via a control system or the field bus. "We need there to be no delay whatsoever in order to ensure that positioning is accurate to 10 µm – even at a cycle rate of 4,000 strokes a minute. The peak values can be attributed to the high computing power of the S700 drives and the generally highly streamlined and uncomplicated programming. Marthiens still looks back fondly at the close collaboration with the Kollmorgen sales team, who were quick to recognize the significance of this invention and also arranged direct contact with Georg Jaskowski, the software developer for the S700 series at Kollmorgen.

Unimagined productivity for the feed process
Kollmorgen CA TecoDrive Servo Drive S700 EN fleXcontrol tecodrive and Kollmorgen have managed to devise a feed method that achieves the kinds of figures that would never be possible with rollers – for one thing, because masses simply cannot be compensated for as quickly as this. By contrast, there is no mass with this feed method, because it only involves a magnetic field. As a result, the process is reduced – in simple terms – to just switching the current on and off, with mass playing no part. This ingenious principle delivers yet more benefits in practice. Switching is silent and does not involve any mechanical stresses. This aspect significantly extends the service life of production equipment in a high-performance environment, as the feed unit is not being exposed to mechanical wear and tear.

Lower energy consumption
Another aspect is currently grabbing the attention of companies active in and around the automotive sector too: the new development only needs a fraction of the energy used by a feed roller. "Although we need to use a Kollmorgen 35 kW servo drive to achieve the necessary magnetizing current, the effective power alone amounts to a mere 700 watts," explains Dr. Olaf Marthiens. For Hans-Jörg Lindner, who manages the business with him, these are further benefits that make the case for abandoning the old methods of feeding materials. "At TriluX, we managed to combine two systems into one. We did this without compromising productivity, and still managed to save lots of space and greatly reduce tool costs." VW at Hanover Stöcken has enjoyed similar positive experiences.

 

Kollmorgen CA TecoDrive Servo Drive S700 EN Linder

Download as PDF

S700

For many years now, this has been one of our most powerful and feature rich servo drives offering:

  • 110 – 480 VAC, 1 or 3-phase, 50 – 60 Hz, up to 72A continuous
  • Legacy bus support including PROFINET, DeviceNet, PROFIBUS DP, SERCOS II and RS232
  • EtherCAT, CANopen fieldbus support
  • Optional functional safety up to SIL3
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Motion Control for intelligent hydraulics

Motion Control for intelligent hydraulics >

KOLLMORGEN develops a standardized servo solution for fluids applications.
Success story: To get the casting die oscillating

To get the casting die oscillating >

What's new in continuous casting: SMS Concast develops actuator-driven oscillation with direct drives by KOLLMORGEN.
Servo drives simulate road behavior

IMS Gear - Servo drives simulate road behavior >

IMS Gear relies on KOLLMORGEN’s Motion Control solution for its test bench technology.
Kollmorgen Automation and Motion Control - Full line catalog

Kollmorgen Full-line Catalog >

At Kollmorgen, we know that OEM engineers can achieve a lot more when obstacles aren’t in the way. With direct sales, engineering support, manufacturing facilities, and distributors spanning the Americas, Europe, the Middle East, and Asia, we’re…

Ball Racing Developments - Racing Simulators - Kollmorgen parts put BRD in pole position >

Formula One racing teams demand the highest performance from every single component, which is why motion system specialist Ball Racing Developments Ltd uses high quality parts supplied by Kollmorgen.

Distributed Servo Technology Bends Panels into Better Shape >

Challenge: Making a departure from traditional drive architectures in its new P2lean generation of machines, Salvagnini the world’s leading manufacturer of panel bending machines is using distributed servo amplifiers for positioning instead of…
Distributed servo technology bends panels into better shape

Salvagnini - Panel Bending Machines - Distributed servo technology bends panels into better shape >

DECENTRALIZED SERVO SOLUTIONS FOR METAL Distributed servo technology bends panels into better shape Salvagnini simplifies the design of its machines using drive solutions from Kollmorgen   Making a departure from traditional drive architectures…

Protek - Cutting-edge laser machining >

DIRECT DRIVES IN LASER CUTTING MACHINES Cutting-edge laser machining Latest machine-generation with cost-efficient mechanical transmission designs