KAS v3.0 Software is Now Available! >
New Features AKD2G Drive Integration: Single and Multi-Axis drive variants Features not yet available: firmware download, capture, I/O, feedback #2-5 Note: Please contact Kollmorgen for latest AKD2G firmware and KAS software. New PCMM…
Motion Solutions brought into focus >
What use are the best motor and the best converter when they are not capable of delivering their full power together? At the 30th edition of the SPS in Nuremberg, the direction in which drive and automation technology is leading was made clear once…
On track with autonomous 2Gen >
Following the successful launch of the second generation AKM2G servo motors, KOLLMORGEN is now expanding its new range for applications in the low voltage range. The specialist in servo drive technology and Motion Control is responding to increased…
New generation of drives, new opportunities >
Partner event – this time in the Czech Republic: KOLLMORGEN invites to the motor factory in Brno