Skip to main content
press_release | Stainless steel servo motors: first for hygiene -

Europe

|
|
minute read

Hygiene is no longer the sole driver of innovation in the food processing industry. In fact, all of the requirements in terms of cleanliness and food safety in machine design relate primarily to modularity, productivity, durability, and availability. The result is a variety of technical features that KOLLMORGEN has successfully combined in the stainless steel servo motors from the AKMH series. The experts in servo drive technology and Motion Control will be exhibiting their hygienic motors during the IFFA (International trade fair of the meat industry) between May 4 to 9, 2019 at the booth shared with Altra (Hall 9.1/Booth D74).

Hygiene is expected—the only question is how intelligently this requirement is taken into account in machinery and the production facilities. With the stainless steel servo motors from the AKMH series, KOLLMORGEN has succeeded in combining a clean exterior with high drive performance, easy cleaning, and above all, high availability. For instance, the internal structural design effectively removes heat losses outwards. Stainless steel has low thermal conductivity, and so motors made of this material normally have problems in this area. The improved heat removal capacity increases drive performance directly in practical usage, as the synchronous servo motors deliver more output for the same design size.

Heat and cold with rapid changes in temperature - plus plenty of water. This interaction creates a further, more serious effect of condensation in a motor’s interior -particularly in the meat processing industry. This is caused by the temperature-related constant pressure equalization, since the volume of the gases expands with heat and contracts with cold. KOLLMORGEN has found a way around this law of physics with a ventilation function via the motor cable. This ensures that the pressure equalization does not take place locally with the humid air of the meat processing operation, but rather uses the prefered temperature of the control cabinet’s protected atmosphere.

The hygienic motors can easily be adapted to allow installation into existing automation structures, for example to suit an existing feedback format. This means the motor can be selected independently of the existing frequency convertor, which is also a real asset when it comes to updating existing systems.

 

ABOUT KOLLMORGEN: Since its founding in 1916, Kollmorgen’s innovative solutions have brought big ideas to life, kept the world safer, and improved peoples’ lives. Today, its world-class knowledge of motion systems and components, industry-leading quality, and deep expertise in linking and integrating standard and custom products continually delivers breakthrough solutions that are unmatched in performance, reliability, and ease-of-use. This gives machine builders around the world an irrefutable marketplace advantage and provides their customers with ultimate peace-of-mind. 

AKMH Stainless Steel Servo Motor

The stainless-steel motors from KOLLMORGEN’s AKMH series are perfect for integration into the hygienic design of machines in the meat processing industry and for retrofitting of existing systems.

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More