WorkBench Minimum Requirements
The detailed requirements for each release are indicated in the release notes. In the table below, we list the different versions in which the minimum requirements have changed.
| WB Version | OS | .NET Framework | Comment |
|---|---|---|---|
| 2.19.0.x ... 2.16.0.x | Windows 10 Windows 11 | 4.8.1 | |
| 2.15.0.x | Windows 10 Windows 11 | 4.8.1 | Win 7 and Win 8 compatibility is dropped (the application will not install at all as the .NET framework is not supported by these OS). |
| 2.14.0.x ... 2.10.0.x | Windows 7 Windows 8 Windows 10 Windows 11 | 4.8 | |
| 2.9.0.x ... 2.4.0.x | Windows 7 Windows 8 Windows 10 | 4.8 | |
| 2.3.0.x ... 1.16.x | Windows 7 Windows 8 Windows 10 | 4.6.1 | |
| 1.15.0.x | Windows 7 Windows 8 Windows 10 | 4.6.1 | XP and Vista compatibility is dropped (the application will not install at all as the .NET framework is not supported by these OS). If you need to run WB on one of these OS, please use the 1.14.0.x release. |
| 1.14.0.x ... 1.8.0.x | Windows XP Windows Vista Windows 7 Windows 8 Windows 10 | 4.0 | |
| 1.7.0.x ... 1.5.0.x | Windows XP Windows Vista Windows 7 | 4.0 | |
| 1.4.0.x ... 1.3.0.x | Windows XP Windows Vista Windows 7 | 2.0 |
Home >
Knowledge Base >
FAQs >
Downloads >