Skip to main content

Kollmorgen Support Network

What is the max. value for motor temperature sensor (PTC)? | 07 Nov 2013 | |

What is the max. value for motor temperature sensor (PTC)?

That depends on the servo amplifier that is used.

S300 5.0 kOhm
S400 2.0 kOhm
S600 1.6 kOhm
S700 5.0 kOhm

About this Article

Kollmorgen Support