Skip to main content

Kollmorgen Support Network

PxMM: Sending and Receiving Variable values via UDP | 30 Jun 2016 | |

PxMM: Sending and Receiving Variable values via UDP

The udpSendToVar and udpRcvFromVar functions  (starting in soon to be released KAS version 2.11)can be use to read and write variables via UDP to and from a PxMM.  The other device can be a PDMM or a third party device. In this example, for ease of testing, data was sent back to the same PDMM with Address 10.8.41.45 using UDP port # 20.


The attached project can be run in a single PDMM and shows the 2 way communications.

Send Program in the project: UDP_Send

image

 

Receive Program in the project: UDP_Receive

image

 

 

To run the program change the IP address in the dictionary to the IP address of the PDMM. Example:

image

 

After starting the project from the IDE , to start the data transfer: Set StartSending =  TRUE:

image

 

The sent data is in the Data Structure is called : Send_Struct_OfData

The received data is in the  Data Structure is called : Received_Struct_OfData

To test,  the data sent can be viewed and changed  in the Watch Window of the attached project:

image

 

Sent Data expanded:

image


Received Data expanded:

image

 

 

The IDE Watch window can be used to change data values in the Send_Struct_of_Data and then observed in the Received_Struct_of_Data

image

image

 

 

 

 

 

 

 

 

 

About this Article

C Wontrop